×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 78452068, Entry date: 01/16/2014
(0)
Rate

SINUMERIK 828D, 840D sl: CYCLE996 example part indexing table

  • Entry
  • Associated product(s)

Description
The task of the CYCLE996 measuring cycle is to simplify the procedure when determining geometrical vectors. The machine kinematics are defined by the geometrical vectors. For measurement purposes, a calibration sphere is mounted on the part indexing table. The principle of this measurement version is that three swivel positions of the calibration sphere are measured for each rotary axes using a probe. The axis vectors in this plane can be calculated from this data. The part indexing table (see Figure) has a rotary axis; as a consequence, only three swivel positions are required when making the measurement. The kinematics are automatically calculated immediately after the rotary axis vectors have been measured.

Advantages of this solution
The solution based on the CYCLE996 presented here has the following advantages:

  • Detailed knowledge about the mechanical system of the machine is not necessary
  • Measurement is realized without dimension drawings and design drawings of the machine
  • The swivel positions of the calibrations sphere do not have to be manually approached
  • Less time is required when determining the axis vectors, by up to one day

Downloads

Content of downloads

Download

Documentation 78452068_Cycle996_example_part_indexing_table_DOKU_V10_en.pdf ( 17651 KB )

Last changes
V1.0, 12/2013, first version

Additional keywords
motioncontrol_cnc_applications

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.