×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 78453460, Entry date: 08/02/2013
(83)
Rate

Download of the PC Adapter USB A2 Driverdisk V1.0

  • Entry
  • Associated product(s)
Description In case you have lost the Driverdisk enclosed with the PC Adapter USB A2, you now have the possibility of a free download of the CD contents. ...

Description

In case you have lost the Driverdisk enclosed with the PC Adapter USB A2, you now have the possibility of a free download of the CD contents.

The Driverdisk V1.0 is applicable to the following operating systems:

  • Windows XP SP2/3, Vista, 7
  • Windows Server 2003, 2008 R2.

SIMATIC software released for later operating systems already includes the necessary drivers for operation.

Procedure

Unpack the file PC_Adapter_USB_A2_Driverdisk_V1_0.zip into a folder on your hard drive and start the setup.exe.

 

Information concerning the Open Source software components

The PC Adapter USB A2 Driverdisk also includes Open Source software components.


Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS file.

Special information for resellers

The information and the license terms in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  ReadMe_OSS.html (579,2 KB)


 

Download

PC_Adapter_USB_A2_Driverdisk_V1_0.zip ( 67144 KB )

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.