×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 78603756, Entry date: 08/13/2013
(2)
Rate

How do you proceed after loading of the F program is aborted with error message D242?

  • Entry
  • Associated product(s)

Description
When loading the F program in TIA V11 Safety Advanced the error message 0xD242 is displayed when a function block cannot be linked.

Cause and remedy
If you are using a CPU 41x-F with a memory card (flash):

  • Check whether the pins are bent.
  • Do not load the program directly into the CPU 41x-F, but into the memory card (flash) ("Online > Download User Program to Memory Card").

If you are using an F CPU for ET 200S:

  • Check whether the pins are bent.
  • Check that the order number of the F CPU used is the same as that of the F CPU configured.
  • Make sure that the termination module for the ET 200S is actually slotted.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.