×
Siemens Industry Online Support
Siemens AG
文档类型 应用实例与扩展工具 文档编号 78604785, 文档发布日期 2020年5月7日
(52)
评估

Standard PCS 7 and WinCC/S7 Water Templates for the Water Industry

  • 文档
  • 涉及产品
The Standard PCS 7 and WinCC/S7 Water Templates provide tailor-made templates for realizing small as well as more complex plants for the water industry. The templates are pre-configured and contain all typical components, their open- and closed-loop controls, required logics, interlocks and visualizations.

The main focus of the water industry lies on these sectors:

  • Drinking water
  • Wastewater
  • Desalination
  • Irrigation
  • Water transport


Fig. 1

The water industry is closely connected to our environment. During its process-related processing it presents technical as well as economic and environmental requirements.

The reduction of servicing and maintenance times as well as the cost savings in planning, engineering, commissioning and training are just as important as the total costs incurred during the entire life cycle of an investment (Total Cost of Ownership = TCO).

Solution
The technical requirements are focused on scalable solutions. The Standard PCS 7 and WinCC/S7 Water Templates provide the possibility to create solutions with CPU S7 IM151-8/S7-300/S7-400/-410(E) hardware in SIMATIC PCS 7 as well as in WinCC/STEP 7.
High availability is guaranteed at all times and at all levels. The implementation of reliable instrumentation as well as the simple integration of energy distributions, drives, shifters, valves and frequency converters have also been taken into consideration.
Even the connections of decentralized structures (pump stations, sewer systems, water storage, storage channels, rain water collection basins, etc.) via remote control technology (TeleControl for PCS 7/-WinCC) e.g. via SINAUT ST7 protocol is an additional important aspect.

The core of the Standard PCS 7 and WinCC/S7 Water Templates is made up of three standard libraries:

  • SIMATIC PCS 7 Advanced Process Library (APL) alternative
  • SIMATIC WinCC/STEP 7 incl. SIMATIC S7 CFC option package 
  • SIMATIC PCS 7-/S7 Industry Library (IL)

To extend the functionality, the following components and libraries are used:

  • SIMATIC PCS 7 PowerControl (Switchgear automation with PCS 7)
  • SIMATIC PCS 7 TeleControl (Controlling of distributed process areas)
  • SITRANS Library (Integration of SITRANS field devices in PCS 7)
  • SITOP Library (Integration of 24V Power supplies in PCS 7)


The predefined water-specific templates are composed of various technological modules and are based on the recommendations of the NAMUR NE33 and ISA S88.1 standards.  


Fig. 2

The standard PCS 7 and WinCC/S7 Water Templates focus mainly on their use by communal or private system operators in the water industry. Sub-systems in the chemical, pharmaceutical, paper, mining or food and beverage industries can be also integrated together with their specific industrial water systems.

Benefits of using the Standard PCS 7 or WinCC/S7 Water Templates

  • Cost reduction during planning and configuring
  • Standardization of water-specific solutions through unified program structures
  • Secure control and monitoring thanks to a uniform look and feel
  • Life cycle warranty with short maintenance and service times

Procurement of the Standard PCS 7 and WinCC/S7 Water Templates
The Standard PCS 7 and WinCC/S7 Water Templates can be procured free of charge from your regional SIEMENS Sales Partner. The downloads include a PCS 7 project archive for the S7 and the PCS 7 Water Templates, profiles for all WCMT and WEMT and hardware circuit diagrams for connecting SIMOCODE motor management systems and general drives.

Documentation
Valid for PCS 7 V9.0 SP2 only with UpdateCollection03
  Standard PCS 7 Water Templates for the water industry with S7-400 hardware (8,8 MB)

Valid for WinCC V7.4/STEP 7 V5.6 incl. S7 CFC V9.0
  Standard WinCC/S7 Water Templates for the water industry for IM151-8(F) and S7-300 Hardware (19,9 MB)

Further information - application examples
Standard PCS 7 and SIMIT Water Templates in the Water Industry

Further information - used components and libraries
Sales and Delivery Release: SIMATIC PCS 7 Industry Library V9.0
Sales and Delivery Release: SIMATIC PCS 7 PowerControl V9.0 
Sales and Delivery Release: SIMATIC PCS 7 TeleControl V9.0
SITRANS Library - Software for integration of the SITRANS product family in SIMATIC
SITOP Library for SIMATIC PCS 7

Documentation for previous versions
Valid for PCS 7 V9.0 SP1
 Standard PCS 7 Water Templates for the water industry with S7-400 hardware (8,1 MB)
 Standard S7 Water Templates for the water industry with S7-300 and IM151(F) hardware (7,8 MB)

Valid for PCS 7 V8.2 with CFC V8.2 Upd3.
 Standard PCS 7 Water Templates for the water industry for PCS 7 and S7-400 hardware (31,4 MB)
 Standard S7 Water Templates for the water industry for PCS 7, IM151-8(F) and S7-300 hardware (28,2 MB)

Valid for WinCC V7.4/STEP 7 V5.5 SP4 incl. S7 CFC V8.2 Upd3
  Standard WinCC/S7 Water Templates for the water industry for IM151-8(F) and S7-300 Hardware (14,3 MB)


Last changes
Update of the standard PCS 7 Water Templates for the water industry with S7-400 hardware to PCS 7 V9.0 SP2

Additional Keywords
water_wastewater, W&WW, WCMT, WPTT, WEMT, water library

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
评估文档
无评估
请求和反馈
您想要做什么?
注意:反馈总是与当前的条目/产品相关。您的消息将被转发给我们在线支持团队的技术编辑们。如果我们需要就您的反馈提供答复,您将在几天内收到答复。如果没有其它问题,您将不会收到答复。