Firmware update for ET200MP IM155-5 PN ST
-
Entry
-
Associated product(s)
Description:
When firmware is updated, it must always be updated to the latest version available for the relevant article number. The previous versions of the firmware are only intended as a backup to enable you to downgrade to the original version.
|
The current PROFINET certificates for ET 200MP are provided here: Certificates
The current GSDML file for PROFINET can be downloaded here: 68189683
Overview of article numbers and current revision levels of the ET200MP IM155-5 PN ST:
Article number | Software | Upgrade by means of... |
---|---|---|
6ES7155-5AA00-0AB0 | ||
V4.1.0 | For upgrade: For STEP 7 TIA Portal | |
V3.0.1 | Backup only: For STEP 7 as of version 5.5 For STEP 7 TIA Portal: | |
V3.0.0 | Backup only: For STEP 7 as of version 5.5 For STEP 7 TIA Portal | |
V2.0.1 | Backup only: For STEP 7 as of version 5.5 For STEP 7 TIA Portal | |
V2.0.0 | Backup only: For STEP 7 as of version 5.5 For STEP 7 TIA Portal | |
V1.0.0 | Backup only: For STEP 7 as of version 5.5 For STEP 7 TIA Portal |
Update V4.1.0 |
Optimization of the diagnostic response
Update V3.0.1 |
The following changes have been implemented:
Reaction to interruption of the MRP ring has been optimized
Reaction to parameterization errors with GSDML configuration has been improved
Update V3.0.0 |
The following functions have been optimized:
- Behavior with high NRT loads
- IM switch-on scenarios in the submodule configuration environment
Update V2.0.1 |
The following changes have been implemented:
- Optimization of the module startup with configurations containing lots of submodules
- Optimization of the module startup with configurations using isochronous mode
Update V2.0.0 |
The following new functions have been implemented:
- Configuration control (option handling)
- Shared Device at submodule level with S7-1500 IO modules (as from Firmware Version V2.0.0)
- German
- Spanish
- Chinese
- Italian
Entry belongs to product tree folder(s):
- Automation Technology Automation Systems Industrial Automation Systems SIMATIC I/O systems ET 200 systems for the cabinet ET 200MP Interface Modules IM 155-5 PN
- Automation Technology Products for specific requirements Automatision technology for extreme conditions SIPLUS extreme Industrial Automation Systems Controllers SIPLUS Advanced Controller SIPLUS S7-1500 SIPLUS Central Processing Units SIPLUS Standard CPUs
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry