Entry type: Download, Entry ID: 78649055, Entry date: 07/03/2015
(1)
Rate

Firmware update for S7-1500 DI 16X24VDC HF

  • Entry
  • Associated product(s)
DESCRIPTION: When firmware is updated, it must always be updated to the latest version available for the relevant article number. The previous versions of the firmware are only intended as a backup to enable you to downgrade to the original version if necessary.

DESCRIPTION:

When firmware is updated, it must always be updated to the latest version available for the relevant article number. The previous versions of the firmware are only intended as a backup to enable you to downgrade to the original version if necessary.

A detailed description of performing the firmware update is provided in the entry 78648446

Overview of article numbers and current revision levels of S7-1500 DI 16X24VDC HF:

Article number

Software
version

Update with...

6ES7521-1BH00-0AB0
V2.1.0

Recommended for update:

see description Update V2.1.0

 

For STEP 7 version 5.5

Registrierung notwendig Classic_6ES7521-1BH00-0AB0_V210.EXE (194.0 KB)

For STEP 7 TIA Portal

Registrierung notwendig TIA_6ES7521-1BH00-0AB0_V210.EXE (194.0 KB)

V2.0.1

Backup only:

see description Update V2.0.1

 

For STEP 7 version 5.5

Classic_5211BH00_V201.EXE ( 189 KB )

For STEP 7 TIA Portal

TIA_5211BH00_V201.EXE ( 259 KB )

V2.0.0

Backup only:

see description Update V2.0.0

 

For STEP 7 version 5.5

Classic_5211BH00_V200.EXE ( 188 KB )

For STEP 7 TIA Portal

TIA_5211BH00_V200.EXE ( 258 KB )

V1.0.0

Backup only:

 

For STEP 7 version 5.5

Classic_5211BH00_V100.EXE ( 186 KB )

For STEP 7 TIA Portal

TIA_5211BH00_V100.EXE ( 254 KB )

 

Update V2.1.0

V2.1.0 contains the following functional optimizations as compared to the previous version:

  • Control of the channel status LED without parameter assignment

V2.1.0 also contains the following functional extension:

  • As an option, two inputs can be used for simple counting functions

 

Update V2.0.1

The following behavior was corrected:

There can be a sporadic, short-term falsification of the input data when operating the module downstream from the PROFINET IM (configuration via GSDML) and a configuration with multiple submodules with short input delays (<= 400µsec).

Update V2.0.0

V2.0.0 contains the following new functions as compared to the previous version:

  • Module-intern shared input/output (MSI/MSO) for shared device
  • Configurable submodule e.g. for shared device
  • Configurable downstream from a IM 155-5 DP ST