Entry type: Download Entry ID: 78683919, Entry date: 08/14/2015
(13)
Rate

Updates for STEP 7 V12 SP1 and WinCC V12 SP1

  • Entry
  • Associated product(s)
Update 5 ( Aug 2015)


Update 5

This update is applicable to the following products:

  • STEP 7 Basic/Professional V12 SP1
  • WinCC Basic/Comfort/Advanced/Professional V12 SP1

Enhancements compared to earlier versions:

STEP 7 Basic/Professional:

WinCC Basic/Comfort/Advanced/Professional:

The readme file for Update 5 is available   here. (186,4 KB).

Installation instructions:

  • Update 5 is cumulative and includes all previous updates.
  • The update can only be installed, if one of the above products is installed already.
  • After each installation of STEP 7 V12 SP1 or WinCC V12 SP1 the latest update must be installed.


Update 5 for STEP 7 / WinCC V12 SP1 (08/2015):
  SIMATIC_TIAP_V12_0_SP1_UPD5 (276,8 MB)

_______________________________________________________________________________ 


Update 4

This update is applicable to the following products:

  • STEP 7 Basic/Professional V12 SP1
  • WinCC Basic/Comfort/Advanced/Professional V12 SP1

Enhancements compared to earlier versions:

STEP 7 Basic/Professional:

  • Reloading a S7-1500 PLC with V12 SP1; a S7-1500 PLC loaded once with TIA Portal V13 can now be loaded again with TIA Portal V12 SP1 at a later time.
  • Stability when working with the TIA Portal has been improved.
  • The maximum number of log entries under "Common data > Logs" has been increased from 5000 to 20000. 

WinCC Basic/Comfort/Advanced/Professional:

  • Dynamic logon is possible for Runtime Professional even if the project was transferred with the function "Load project to a file system".

The readme file for Update 4 is available here (182 KB) ( 182 KB ) .

Installation instructions:

  • Update 4 is cumulative and includes all previous updates.
  • The update can only be installed, if one of the above products is installed already.
  • After each installation of STEP 7 V12 SP1 or WinCC V12 SP1 the latest update must be installed.


Update 4 for STEP 7 / WinCC V12 SP1 (03/2014):
 SIMATIC_TIAP_V12_0_SP1_UPD4.exe (203663 KB) ( 203663 KB )   

_______________________________________________________________________________ 

Update 3

This update is applicable to the following products:

  • STEP 7 Basic/Professional V12 SP1
  • WinCC Basic/Comfort/Advanced/Professional V12 SP1

Enhancements compared to earlier versions:

STEP 7 Basic/Professional:

  • Internal parameter of a GRAPH block can be declared as retentive.
  • Stability during creation of SCL programs has been improved.
  • The accessibility of devices connected to the programming device/PC online via an interface has been optimized.
  • Performance when working with libraries has been increased.
  • Stability when working with the TIA Portal has been improved.

WinCC Basic/Comfort/Advanced/Professional:

  • The routines for displaying references and for rewiring have been improved.
  • With faceplates for Panels and Runtime Advanced, function lists can be triggered by a change to an interface event.
  • References to tags can also be transferred to Runtime Advanced for ActiveX controls.

The readme file for Update 3 is available here ( 141 KB )   .

Installation instructions:

  • Update 3 is cumulative and includes all previous updates.
  • The update can only be installed, if one of the above products is installed already.
  • After each installation of STEP 7 V12 SP1 or WinCC V12 SP1 the latest update must be installed.


Update 3 for STEP 7 / WinCC V12 SP1 (12/2013):
 SIMATIC_TIAP_V12_0_SP1_UPD3.exe ( 188423 KB )  

_______________________________________________________________________________ 

Update 2

This update is applicable to the following products:

  • STEP 7 Basic/Professional V12 SP1
  • WinCC Basic/Comfort/Advanced/Professional V12 SP1

Enhancements compared to earlier versions:

STEP 7 Basic/Professional:

  • The instruction "SETP: Set bit field in the I/O area" and "RESETP: Reset bit field in the I/O area" for S7-400 has been expanded in accordance with the Online Help System.
  • The stability in the use of library elements has been improved.

WinCC Basic/Comfort/Advanced/Professional:

  • The processing of tags in VB-scripts has been improved.
  • System diagnostics: The stability and the consumption of resources in Runtime has been improved.

The readme file for Update 2 is available here (88 KB) ( 88 KB ) .

Installation instructions:

  • The update can only be installed, if one of the above products is installed already.
  • After each installation of STEP 7 V12 SP1 or WinCC V12 SP1 the latest update must be installed.


Update 2 for STEP 7 / WinCC V12 SP1 (08/2013):
 SIMATIC_TIAP_V12_0_SP1_UPD2.exe (75039 KB) ( 75039 KB )

_______________________________________________________________________________ 

Update 1

The Update 1 of TIA Portal V12 SP1 is reserved for system purposes and is not available to TIA Portal users.
 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.