×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 78794562, Entry date: 08/19/2013
(0)
Rate

What is the purpose of the YL connector on the RGJ ramp-function generator block?

  • Entry
  • Associated product(s)

Description
With the "RGJ" block of the "D7-SYS" configuration software the input connectors LU (Upper Limit) and LL (Lower Limit) do not affect the output connector Y, but the input connector X, so that there can always be jerk limiting.
Therefore it is possible that output Y can also have values that are beyond the range defined by LU and LL.

Instructions
When using the "RGJ" block you should usually use the YL connector (with integrated output value limitation).
At this output the output value is automatically limited to the range defined by the user with the input connectors LU and LL.

If you nevertheless use the output connector Y, pleasure use appropriate switching to ensure that the value of the output connector Y remains in the range you want.

Additional information about "RGJ" is available in the "Reference Manual" of the D7-SYS function blocks in Entry ID 14952400.

Additional Keywords
Ramp-function generator, Ramp

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.