×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 79047707, Entry date: 03/23/2017
(16)
Rate

Closed-Loop Control of Simulated Controlled Systems in the S7-1500 with PID_Compact V2

  • Entry
  • Associated product(s)
This entry provides you with a block library for simulating controlled systems for the SIMATIC S7-1200 and S7-1500 controller families. It additionally provides you with a sample project for the S7-1500 in conjunction with the “PID_Compact” technology object, V2.2. Handling the library and the software controller is documented in detail.

Task
Influencing technical variables in systems requires controlling these variables. In automation technology, controllers are used in many different ways, for example for temperature control in processes. In this example, the automation task is to set up a control loop for influencing simulated physical parameters in a technical process.

The control loop is to consist of the following elements:

  • “PID_Compact” V2.x as the controller used as a basis.
  • Technical processes simulated in the S7 CPU as the controlled system.

Solution
To demonstrate the application task, a closed-loop control system is implemented by the S7-1500 with the aid of the “PID_Compact” block and the “LSim” simulation library. The PC station is used for visualizing the control loops, the PG is used for configuring.


Figure 01

Advantages
This application provides the following advantages:

  • Step-by-step description for first commissioning of a “PID_Compact” controller
  • Quick way to get started handling the functions of “PID_Compact”
  • Saves time and costs by simulating controlled systems with the aid of the “LSim” controlled system library

Downloads
  Documentation: “Library for Controlled System Simulation with STEP 7 V14 (TIA Portal)” (1,5 MB)
 Registrierung notwendig  STEP 7 V14 (TIA Portal) “LSim” Block Library (501,6 KB)
 Registrierung notwendig  Documentation: “Closed-Loop Control with PID_Compact V2.3” (1,9 MB)
 Registrierung notwendig  TIA Portal V14 Sample Project “S7-1500 with PID_Compact V2.3” (1,4 MB)

  Documentation: “Library for Controlled System Simulation with STEP 7 V13 SP1 (TIA Portal)” (1,5 MB)
 Registrierung notwendig  STEP 7 V13 SP1 (TIA Portal) “LSim” Block Library (1,1 MB)
 Registrierung notwendig  Documentation: “Closed-Loop Control with PID_Compact V2.2” (1,9 MB)
 Registrierung notwendig  TIA Portal V13 SP1 Sample Project “S7-1500 with PID_Compact V2.2” (7,3 MB)

Further Information
Function Manual: “SIMATIC S7-1200/S7-1500 PID Control”
Application Example: “Single and Multi Loop Controller Structures (Cascade Control) with PID_Temp”
Application Example: “3-Point Stepper Control with SIMATIC S7-1500”
Application Example: “PID Control with PID_Compact (S7-1200)”
Application example "Multi-Zone Control with PID_Temp for SIMATIC S7-1200/S7-1500"

Last Changes

  • Optimizing of library block "LSim_Lagging"
  • Adding library block "LSim_Multizone" for STEP 7 V14
  • Update to “PID_Compact” V2.3 (TIA V14)


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit