×
Siemens Industry Online Support
Siemens AG
文档类型 产品通知 文档编号 79719037, 文档发布日期 2013年10月15日
(0)
评估

Delivery release: New ground fault module for SIMOCODE pro V

  • 文档
  • 涉及产品

High-precision ground fault monitoring – the new ground fault module for SIMOCODE pro V represents the highest standard on the market.

Date for the Release for Delivery : 2013-09-30


Product description:
External earth fault monitoring is usually carried out in networks which are grounded at high impedance and in cases where exact measurement of the earth fault current is necessary, e.g. for condition monitoring purposes. Thanks to our new earth fault module 3UF7510-1AA00-0, we are able to offer the optimum solution in combination with the SIMOCODE pro V range and the 3UL23 residual current transformer.

The highlights of our solution, which enable increased plant availability, include:
- Fault current limit selectable within a large range
- High measuring accuracy
- Connection of transformers with large feed-through openings up to 210 mm
- Adjustable warning and tripping limits
- Permanent monitoring for open circuit and short circuit of the connection from the
  residual current transformer to the earth fault module

Furthermore, combining the new earth fault module 3UF7510-1AA00-0 with the 3UL23 residual current transformer represents better value than the previous solution for all feed-through opening sizes.

There are predecessor types: How is the detachment imaginary?
The predecessor model 3UF7500-1AA00-0 will be discontinued as of June 2014. Replacement units will continue to be available beyond this date.

Differences compared with predecessor types:
The dimensions and functions of the new earth fault module 3UF7510-1AA00-0 are fully compatible with those of its predecessor, 3UF7500-1AA00-0, and can be used with pro V basic units from product versions E10 (PROFIBUS) or E04 (PROFINET) onwards, both of which have been available since September 2013.

Ordering data:
3UF7510-1AA00-0, ground fault module for SIMOCODE pro V   

In combination with the 3UL23 residual-current transformer, the new ground fault module permits the measurement and notification of the ground fault current to the control system with the following functions:
- parameterizable residual current limit within the range from 30 mA to 40 A
- high measurement accuracy (accuracy of ± 7.5%)
- 1 transformer per outlet opening (regardless of fault current)
- possible outlet openings of 35 mm, 55 mm, 80 mm, 105 mm, 140 mm, 210 mm
- permanent self-monitoring of the ground fault module and monitoring of the connection
  of the transformer to the ground fault module

Listed below are the order numbers of the 3UL23 residual-current transformers that can be connected to the ground fault module:
 

Order number

Opening diameter

3UL2302-1A

35 mm

3UL2303-1A

55 mm

3UL2304-1A

80 mm

3UL2305-1A

110 mm

3UL2306-1A

140 mm

3UL2307-1A

210 mm

The new ground fault module can be used with pro V basic units from product versions E10 (PROFIBUS) or E04 (PROFINET) onwards, both of which have been available since September 2013.

SIMOCODE ES 2007 software(Service Pack 5) can be used for parameterization.
Service Pack 5 for SIMOCODE ES 2007 can be downloaded from the following location:
http://support.automation.siemens.com/WW/view/en/79605509

Further information on SIMOCODE can be found online at:
www.siemens.com/simocode

 

 


安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
评估文档
无评估
请求和反馈
您想要做什么?
注意:反馈总是与当前的条目/产品相关。您的消息将被转发给我们在线支持团队的技术编辑们。如果我们需要就您的反馈提供答复,您将在几天内收到答复。如果没有其它问题,您将不会收到答复。