SINAMICS S120: Controlling Safety Integrated Extended Functions and transferring the F-DIs of the CU310-2 PN via PROFIsafe with PROFINET
-
Entry
-
Associated product(s)
Task
A modular safety concept is to be presented in
this example. Sensors locally connected at the F-DIs of the drive
only control safety functions SS1 and SLS for this particular
drive. Sensors directly connected to the F-DI modules of the F-CPU,
control the SS1 and SLS safety functions for all drives of a
machine. PROFIsafe via PROFINET is always used for the control. To
do this, the signals of the sensors connected to the F-DIs of the
SINAMICS S120 are transferred to the F-CPU using PROFIsafe, where
they are subsequently evaluated.
Solution
Controlling safety functions SS1 and SLS via PROFIsafe with PROFINET for a SINAMICS S120 drive line-up is demonstrated using this application example. The S120 drive line-up used comprises a Control Unit CU310-2 PN, a Power Module PM340 and a 1FK7 servomotor with incremental Drive-CLiQ encoder.
In order to be able to implement a modular safety concept, in
this particular example, the safety functions are locally
controlled (only effective for this drive) and globally controlled
(effective for all drives of a system/machine). The local safety
functions are controlled using sensors at the F-DIs of the drive.
These sensors only control the SS1 and SLS safety functions for
this particular drive. The local, safety-relevant signals are
transferred from the fail-safe onboard terminals of the SINAMICS
S120 via PROFIsafe with PROFINET to the F-CPU. The other global
safety functions are controlled using the sensors of the SAFETY
training case. These global signals are sensed using the fail-safe
inputs of the F-CPU. They control the SS1 and SLS safety functions
for all of the drives of a machine.
All of the signals detected and transferred at the F-CPU are
evaluated in the F-CPU, and logically interlocked in the safety
program to allow the integrated SS1 and SLS safety functions to be
controlled.
The safety functions integrated in the SINAMICS S120 drive being
used are controlled using fail-safe PROFIsafe communication. The
F-CPU is the F host as well as also the PROFINET controller.
Downloads
Content of downloads |
Download |
Documentation | ![]() |
Project | ![]() |
History
V1.0, First Edition
Additional search terms
motioncontrol_apc_applications
- German
- Spanish
- French
Entry belongs to product tree folder(s):
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry