×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 79993228, Entry date: 06/30/2017
(1)
Rate

Which SNMP requests can the S7-1500 CPUs and S7-1200 CPUs receive and reply to?

  • Entry
  • Associated product(s)
The S7-1500 CPUs and S7-1200 CPUs support the transfer of management information over the Simple Network Management Protocol (SNMP). The S7-1500 CPUs and S7-1200 CPUs can receive and reply to SNMP requests?

Information about the properties of SNMP-compatible devices is available in the so-called MIB files (Management Information Base). The S7-1500 CPUs und S7-1200 CPUs reply to the SNMP tags of the following MIBs:

Note

  • The S7-1500 CPUs und S7-1200 CPUs do not have private MIBs.
  • The S7-1500 CPUs and S7-1200 CPUs cannot access the SNMP tags of other devices, because they cannot send or request SNMP commands. They can receive and reply to SNMP requests.

  • Only the SNMP tags sysName, sysContact and sysLocation can be written in MIB II. All other SNMP tags can only be read.

Further Information
A sample application for monitoring and controlling network components with an S7 PN CPU as SNMP Manager is available in Entry ID 57249109.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit