Entry type: FAQ, Entry ID: 814230, Entry date: 04/26/1999
(0)
Rate

Using function key F10 with an FI45

  • Entry
  • Associated product(s)

QUESTION:
How can I use the function key F10 with an FI45 with ProAgent?

ANSWER:
If you use this key with an FI45 project with WinCC ProAgent, then you must install the file available here for downloading. This file contains the parameterization required.

Procedure:
Copy the WCC_FI45.EXE file into a separate directory and then start it with a double-click. Copy the extracted PAWinCC_.key file into the "...\Keyboard" directory of the FI45. Using the tool KEYLIGHT (in the \Keyboard catalog) you can activated the new Key file. For more details see the FI45 instruction manual.

Wcc_fi45.exe (18 KB)