×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 82140974, Entry date: 10/18/2013
(0)
Rate

Compatibility of VPN connections between Industrial Ethernet products with Security Integrated and CP 1543-1, via infrastructure in which Network Address Translation (NAT) is being used.

  • Entry
  • Associated product(s)

 

The CP 1543-1 (6GK7543-1AX00-0XE0) supports the VPN functionality as from firmware version V1.1.15.

The active establisment of a VPN connection between Security Integrated products and CP 1543-1 via infrastructure in which Network Address Translation (NAT) is being used will work as from the following firmware versions of the products:

 

Product

Order Number

Firmware Version

Delivery Release

SOFTNET Security Client

6GK1704-1VW04-0AA0

≥ V 4.0

09/11

SCALANCE M875

6GK5875-0AA10-1AA2

V 2.116

12/12

SCALANCE S612

6GK5612-0BA10-2AA3

≥ V 4.0

09/13

SCALANCE S623

6GK5623-0BA10-2AA3

≥ V 4.0

09/13

CP 443-1 Adv

6GK7443-1GX30-0XE0

> V 3.1.7

09/13

CP 343-1 Adv

6GK7343-1GX31-0XE0

> V 3.0.33

mid 2014

CP 1628

6GK1162-8AA00

≥ V 8.2.12

09/13

Table 1

 

 

 

The following Security Integrated products cannot actively establish a VPN connection to a CP 1543-1 via infrastructure with NAT:

 

Product

Order Number

SCALANCE S612

6GK5612-0BA00-2AA3

SCALANCE S613

6GK5613-0BA00-2AA3

Table 2

 

If the CP 1543-1 actively establishes a VPN connection to a Security Integrated product via infrastructure with NAT, the data exchange will be without any problems, irrespectively of the firmware used by the partner. By default both parties to a VPN connection are always active, this can be suitably adapted by configuration.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.