×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 82169157, Entry date: 01/24/2017
(26)
Rate

In STEP 7 (TIA Portal) V13 SP1, how do you load project data from a device that has been configured with STEP 7 (TIA Portal) V12 SP1 or V13?

  • Entry
  • Associated product(s)
If, in STEP 7 (TIA Portal) V13 SP1, you load project data from a device that you have previously loaded into the device using a previous version of STEP 7 (TIA Portal) V1x, you must open "Compatibility Mode V1x".

Description

Version 1
The download to the device was done with STEP 7 (TIA Portal) V13

In this case you must use "Compatibility Mode V13". However, this is only possible with an open STEP 7 (TIA Portal) V13 project.
For the case that you do not have a STEP 7 (TIA Portal) V13 project, we have included an empty STEP 7 (TIA Portal) V13 project for downloading in this FAQ response.

Download 1
The download contains the "compatibility_mode_V13_V13SP1" project.
Copy the "82169157_compatibility_mode_V13_V13SP1.zip" file into a separate directory and then start the file with a double-click. You can then use STEP 7 (TIA Portal) to open and process the extracted project data.

Registration required 82169157_compatibility_mode_v13_v13sp1.zip (307.1 KB)

Version 2
The download to the device was done with STEP 7 (TIA Portal) V12

In this case you must use "Compatibility Mode V12". However, this is only possible if a STEP 7 (TIA Portal) V12 SP1 projectis open.
For the case that you do not have a STEP 7 (TIA Portal) V12 SP1 project, we have included an empty STEP 7 (TIA Portal) V12 SP1 project for downloading in this FAQ response.

Download 2
The download contains the "compatibility_mode_V12_V13" project.
Copy the "82169157_compatibility_mode_V12_V13.zip" file into a separate directory and then start the file with a double-click. You can then use STEP 7 (TIA Portal) to open and process the extracted project data.

Registration required 82169157_compatibility_mode_v12_v13.zip (291.6 KB)

Note on STEP 7 (TIA Portal) V12 SP1
If, in STEP 7 (TIA Portal) V12 SP1, you have to do a program upload of a device programmed with STEP 7 (TIA Portal) V11 (a SIMATIC controller, for example), then you have to open "Compatibility Mode V11" for this. Information about this is available in Entry ID: 66027369.

Creation Environment
Download 1 in this FAQ response was created with STEP 7 (TIA Portal) V13 Update 6 and Download 2 with STEP 7 (TIA Portal) V12 SP1 Update 3.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.