×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 82203451, Entry date: 08/15/2019
(24)
Rate

Library for SNTP Server Functionality in SIMATIC S7 CPUs (LSNTP)

  • Entry
  • Associated product(s)
The PROFINET CPUs of the automation systems SIMATIC S7-1200/1500 and S7-300/400 and WinAC RTX can only be configured as NTP clients for time synchronization. With this library you can turn a SIMATIC S7 CPU into an SNTP server and thus realize a simple time synchronization of automation cells.

Solution
In this entry we provide you with library blocks for all current SIMATIC S7 CPUs, which map the functionality of an SNTP server.
The following sample configuration shows a possible use, for example, of an S7-1500 CPU as SNTP server in an automation cell.

The LSNTP_Server function block provides the following functions:

  • Receipt and analysis of an NTP request from a client.
  • Creation and sending of an SNTP message to the requesting client.

Note
For S7-1200 the library is valid for CPU firmware versions up to 3.x and 4.1.3 and higher.

Downloads
TIA Portal V15.1
  Documentation (1,3 MB)
 Registrierung notwendig  Library LSNTP V3.0.2 for TIA Portal V15.1 (614,1 KB)

STEP 7 V5.5
  Documentation (1,0 MB)
 Registrierung notwendig  Library V1.0.0 for STEP 7 V5.5 (37,7 KB)


Last Changes

Replaced DCF77 with generic NTP server in overview graphic

Additional Keywords
Time synchronization, time leveling, NTP server

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.