×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 8250891, Entry date: 07/22/2015
(15)
Rate

Which version of STEP 7 is compatible with which version of Microsoft Windows operating system?

  • Entry
  • Associated product(s)
The Compatibility Tool is a function provided by the Industry Online Support with which you can select compatible software products or check the compatibility of existing configurations.

Compatibility information for STEP 7V5.4 and higher is available in the Compatibility Tool.
You can call the Compatibility Tool in the following entry:
64847781

Please use the new entry for your favorites.

This entry includes the following information:

  • New compatibility information
  • New tool functions
  • Tool operating instructions and help

Compatibility information for lower versions of STEP 7 up to and including V5.3 is available in the list below.

Download
  Kompat_step7_win_e.pdf (47,1 KB)

Note on Windows 2000 Server
STEP 7 is not released for operation in MS Windows 2000 Server.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.