SINAMICS S120: Application example for the "Safely Limited Position (SLP)" function and the "Retraction" block using the EPOS function
-
Entry
-
Associated product(s)
Task
In this example, safety functions SS1E and SLP
should be controlled in conjunction with the EPOS function of the
SINAMICS S120. Safety function SS1E becomes active when Emergency
Stop pushbutton -S1 is pressed. The drive is externally braked
until standstill is reached. It then goes into the STO state.
Based on safe actual value sensing, the drive position values are
available in a safety-related form. When the "Safely Limited
Position (SLP)" safety function is active, the drive cannot exit a
position range that has been configured by the user. When the limit
values are reached, the drive is stopped with the configured stop
response. In order to be able to traverse the drive from a
non-permissible position range, safety function SDI and traversing
the drive in the jog mode are also configured. The drive can be
traversed back into the permissible position range using the
"Retraction" block integrated in the safety program in the F-CPU.
In this particular example, the safety function is controlled via
PROFIsafe with PROFINET.
Solution
Controlling safety functions SS1E and SLP via PROFIsafe with
PROFINET – as well as using the basic positioner (EPOS) – for a
SINAMICS S120 drive is demonstrated using this application
example.
The drive line-up in the booksize format comprises an infeed and a
Double Motor Module (DMM). Position and motor control are realized
using a CU320-2 PN Control Unit. This involves hardware that is
installed in the SINAMICS S120 demonstration cases. The servomotor
is controlled using the Double Motor Module. A Smart Line Module
(SLM) is used as infeed.
The safety-relevant signals are sensed using fail-safe digital
input modules, logically processed in the F-CPU. The F-CPU sends
the fail-safe data to the drive via the PROFIsafe telegram 31,
where it controls the safety functions.
Downloads
Content of Downloads |
Download |
Documentation | |
Code |
Additional search
terms
motioncontrol_apc_applications
- German
- Spanish
- French
- Chinese