×
Siemens Industry Online Support
Siemens AG
文档类型 应用与工具 文档编号 82555461, 文档发布日期 2013年12月11日
(0)
评估

Monitoring 24V load circuits using SITOP PSE200U with single channel message and SIMOTION CPU

  • 文档
  • 涉及产品

Task
Using the SITOP PSE200U selectivity module with single channel message enables you to monitor up to four 24V load circuits for overload or short-circuit. The signal at the state output (S) of the SITOP PSE200U module provides you with serially coded information on the state of the individual load circuits connected to outputs OUT 1 to OUT 4 of the SITOP PSE200U selectivity module. The state of the load circuits shall be detected by a SIMOTION CPU and monitored.

Solution
The entry on hand contains a function block as well as a function description. The function block enables you to read and evaluate the signal of the status output (S) via a digital input at the SIMOTION CPU. A possible application, for example, would be indicating this information as alarm message on a panel.

The figure below shows the graphic representation of the solution.

 

Downloads

Content of Downloads

Download

Function block documentation
 Description of the function block for SIMOTION SCOUT V4.3.1 and SIMOTION CPUs
82555461_PSE_DIAG_Baustein_DOKU_SIMOTION_en.pdf ( 2588 KB )
Code 
ST source (ST = structured text) of the function block for SIMOTION SCOUT V4.3.1 and SIMOTION CPUs
PseDiag.zip ( 3 KB )

Last Changes
New version

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.