×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 82605334, Entry date: 02/26/2020
(7)
Rate

SIMATIC Simapress: Software package to automate a conventional flywheel press

  • Entry
  • Associated product(s)
Automation of a conventional flywheel press with SIMATIC S7-1500

At a mechanical flywheel press following main and additional functionalities are typically needed:

  • Main drive control mechanical press with positioning mode
  • Brake angle calculation
  • Stroke counter
  • Cam controller
  • Die protection
  • Tonnage monitoring
  • Envelope monitoring
  • Visualisation over HMI
  • Machine data handling
  • Die data handling

This application example is intended for all engineers an users that wish to implement a mechanical excentric press based on SIMATIC S7-1500. It realizes all of the above mentioned functionalities based on following hardware: SIMATIC S7-1500, TM Timer, AI HS, SINAMICS S120. 


The hardware design can look like this for example:

MCD/SIMIT model
This application example allows you to simulate the SIMATIC Simapress application in combination with the SIMATIC S7-F/P Press Safety Blocks using PLCSIM Advanced, SIMIT and NX Mechatronics Concept Designer (MCD). Therefore, the MCD Model consists of a mechanical flywheel press and simulates it's kinematics. Furthermore, a SIMIT model is provided to simulate the behavior model for this machine setup and PLCSIM Advanced is used to emulate a SIMATIC S7-1500 controller. The PLCSIM Advanced instance runs the corresponding example project for SIMATIC Simapress. This setup allows a virtual commissioning on the digital twin.


Note
For providing the MCD/SIMIT projects, as well as manual and screencast, please contact your Siemens contact person.
Contacs worldwide



Downloads
  Slides V3.1 10/2017 (2,3 MB) 


Additional search terms
motioncontrol_apc_applications, Umformtechnik, Metalforming

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.