×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 82947835, Entry date: 08/15/2019
(5)
Rate

How do you read out the IP address of the PROFINET interface of a S7-1500 CPU in the user program?

  • Entry
  • Associated product(s)
You can read out the IP address of the PROFINET interface of a S7-1500 CPU from the user program. You can use the PROFINET data records for this.

You can use the PROFINET data records to determine the IP address of the PROFINET interface of an S7-1500 or S7-1200 CPU.
A block library and the associated library description are available in the following entry:
Library for PROFINET data records

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.