×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 82969029, Entry date: 10/31/2013
(1)
Rate

SIMOCODE ES V12 (TIA Portal)

  • Entry
  • Associated product(s)
SIMOCODE ES V12 (TIA Portal): The central software package for the configuration, commissioning, operation, and diagnosis of SIMOCODE pro
SIMOCODE ES V12 is the central software package for the configuration, commissioning, operation, and diagnosis of SIMOCODE pro with PROFIBUS communication interface.
In addition to SIMOCODE ES Version 12, based on the Totally Integrated Automation Portal (TIA Portal) central engineering framework, the software continuously is available as version 2007 for all SIMOCODE pro basic units.
http://support.automation.siemens.com/WW/view/en/79605509?Datakey=27833560

The software is based on the Totally Integrated Automation Portal (TIA Portal) central engineering framework and can be seamlessly integrated if additional TIA Portal-based software such as STEP 7 and WinCC is present, thus providing the user with a consistent, efficient, and intuitive solution to all automation tasks.
But those using SIMOCODE ES V12 as standalone software will also enjoy its benefits.




Three program versions
Users can choose between different versions of SIMOCODE ES: SIMOCODE ES Basic, SIMOCODE ES Standard, and SIMOCODE ES Premium. While SIMOCODE ES Basic is a powerful tool for commissioning or maintenance personnel, a greater functional scope and integrated graphics editor make SIMOCODE ES Standard and Premium perfect tools for engineers and project planners. Unlike the standard version, SIMOCODE ES Premium also allows parameterization and diagnosis via PROFIBUS. The display of all operating, service, and diagnostic data supplies meaningful information about the current state of the motor and the system at all times – everywhere in PROFIBUS.

Integrated graphics editor
The graphics editor is a part of SIMOCODE ES Standard and SIMOCODE ES Premium. It is based on the Continuous Function Chart (CFC) and adds a powerful tool to the parameterizing interface that enables easy parameterization of devices by Drag&Drop. Extremely compact documentation of all configured parameters is possible, as is the graphic online presentation of the configured device functions including all signal states during operation.




Trial License

The software comprises a trial license of SIMOCODE ES V12 Premium. The Licensee shall be granted the non-exclusive and non-transferable right to install the SW in one (1) Instance and to use it for validation purposes in the manner specified in the Order Data or CoL (see "Type of Use"). The period of usage is limited to 21 days and commences with the SW start-up, unless a different period of usage is specified in the Order Data or CoL.



System requirements

Operating system

Windows XP Professional Service Pack 3,
Windows 7 32/64 Bit Professional/Ultimate/Enterprise (Service Pack 1),
Windows Server 2008 32 Bit StdE (Service Pack 2),
Windows Server 2008 64 Bit R2 StdE (Service Pack 1)

Processor

2 GHz (Core 2 Duo)

RAM

1 GB (Windows XP)
2 GB (other operating systems)

Monitor resolution

>=1024 x 768

Grafics cards

32 Mbyte RAM, 24-bit color intensity

Free space on hard disc

2 GB

CD-ROM-/DVD drive

DVD-ROM (only when installing from DVD)

Interface

Depends on PC cabel: serial (COM) or USB

PC cabel/parameterization cabel/connection cabel

Yes

PROFIBUS interface

Optional, for parameterization and diagnostics through PROFIBUS


Installation notes

The software is offered in the form of the download file SIMOCODE_ES_V12.zip. After having unzipped the *.zip file, please read the file Readme.htm first and then run the program Start.exe.

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS file.

Special information for resellers

 The information and the license terms in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing Party.

  Readme_OSS.htm (2,4 MB)

Download  (also contains OSS source code)

SIMOCODE_ES_V12.zip ( 1667269 KB )

Update: Updates for SIMOCODE ES V12 (TIA Portal)


 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.