×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 83130159, Entry date: 01/30/2015
(12)
Rate

How do you program and parameterize Modbus/TCP communication between two S7-1200 CPUs?

  • Entry
  • Associated product(s)
To establish Modbus/TCP communication between two S7-1200 CPUs you call the "MB_CLIENT" and "MB_SERVER" instructions in the user program of the S7-1200 CPUs.

The "MB_CLIENT" instruction communicates as Modbus/TCP client via the PROFINET connection of the S7-1200 CPU. You do not need any additional hardware to use the instruction. You use the "MB_CLIENT" instruction to establish a connection between the client and the server, send requests and receive responses, and control the connection disconnection of the Modbus/TCP server.

The "MB_SERVER" instruction communicates as Modbus/TCP server via the PROFINET connection of the S7-1200 CPU. You do not need any additional hardware to use the instruction. The "MB_SERVER" instruction processes connection requests of a Modbus/TCP client, receives requests from Modbus functions and sends response messages.

The application example and the instructions in Entry 102020340show how to call and parameterize the "MB_SERVER" and "MB_CLIENT" instructions in the user program of the S7-1200 CPU.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.