×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 8338428, Entry date: 09/14/2001
(0)
Rate

GSD files supplied for PROFIBUS DP (CB15/CB155) not correct

  • Entry
  • Associated product(s)

The GSD file supplied for the PROFIBUS DP option CB15/CB155 for MICROMASTER 3 is not up-to-date and can result in errors when it is imported.

The GSD file is part of the documentation CD which is supplied with the option.

The actual GSD file for the PROFIBUS DP option CB15/CB155 is available under the following WEB address:

http://www.ad.siemens.de/csi_e/gsd.

The documentation CD will be updated.

The product includes the documentation CD (respectively Disk) actually labeled with "23.03.01" which contains the relevant GSD-File in the latest version already. This File is identical to the GSD-file to be downloaded from the Siemens Intranet.

If you still have problems, please contact your Customer Support.



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.