×
Siemens Industry Online Support
Siemens AG
Entry ID: 83557459, Entry date: 05/04/2020
(13)
Rate

Migration of plants with SIMATIC (TIA Portal) - Controllers

  • Entry
A certain amount of know-how is required for migrating to new systems. Siemens supports you with many tools and other aids to get successfully into the TIA Portal and the new SIMATIC components.


In order to optimize the performance of a plant, it is useful to check regularly that it is state of the art. A certain amount of know-how is required for migrating to new systems. Siemens supports you with many tools and other aids to get successfully into the TIA Portal and the new SIMATIC components. Here we provide an overview of the relevant topics with links to the most important entries.






 Complete systemsController and IO
Visualization
Communication
TIA Portal

Here you have direct access to the most important technical information and solutions for controllers.


Migrationtools


Migration Tool TIA Portal
In many cases a project that you wish to migrate is not on the same PG/PC as the TIA Portal. The migration tool converts the initial project into a compatible format. You can read this file into the TIA Portal and continue processing it.
TIA Selection Tool
The TIA Selection Tool is for selecting, configuring and ordering devices, software and licenses.


Programming languages


Programming Guidelines and Programming Styleguide for SIMATIC S7-1200 and S7-1500
SIMATIC S7-1200 / S7-1500 Comparison list for programming languages based on the international mnemonics
What should you watch out for when migrating an S7-SCL program in STEP 7 (TIA Portal)?


From STEP 7 V5.x to STEP 7 (TIA Portal)


What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)?
What are the requirements for the migration of STEP 7 V5.x projects in STEP 7 (TIA Portal)?
What are the requirements for installing TIA Portal V17 (STEP 7 Professional / Basic, WinCC Professional / Advanced)?
How do you upgrade projects in TIA Portal V14 and higher that you created with previous versions of TIA Portal?
Why, after project migration from STEP 7 (TIA Portal) V13 SP1, does STEP 7 (TIA Portal) V14 issue the message "The data type Word of the actual parameter does not match the data type HW_IO of the formal parameter"?
Migration of a Safety Program to TIA Portal
How do you efficiently and effectively program for the S7-1200/S7-1500 in STEP 7 (TIA Portal)?
What are the differences in the keyboard operation of STEP 7 (TIA Portal) and STEP 7 V5.x?
SINAMICS G120 / G120D / G120P / G120C: Migration of a STEP 7 Classic project into a STEP 7 V12/V13 project.
Where are the standard blocks and instructions stored in STEP 7 (TIA Portal) and in V5.x (SIMATIC Manager)?
How do you import blocks in a STEP 7 (TIA Portal) project that were created in other projects or with earlier versions of STEP 7?
More information about S7-1200


Licenses


Which license do you need to upgrade from STEP 7 version V5.x, V11 ... V16 to the TIA Portal V17?
What is the difference between authorizations and license keys?


From S7-200 to S7-1200


Making the transition from S7-200 to S7-1200
What has to be considered to replace S7-200 PID applications with "PID_Compact" V2 for S7-1200?
More information about S7-1200


From S7-300/400 to S7-1500


Migration Guide: SIMATIC S7-300/400 to SIMATIC S7-1500
Migration Guide: S7-31xT to S7-1500(T)
PLC migration to S7-1500 with STEP 7 (TIA Portal)
Which entries are available in the internet concerning migration to STEP 7 (TIA Portal) and WinCC (TIA Portal)?
How can you migrate alarms in the TIA Portal from the S7-300/400 to the S7-1500?
To which differences should you pay attention in the case of retention when you migrate a GRAPH-FB in STEP 7 (TIA Portal) from S7-300/S7-400 to S7-1500?
What should you watch out for when you migrate the AG_SEND/AG_LSEND instruction from the user program of the S7-300/S7-400 in the TIA Portal to the user program of the S7-1500?
How do you implement module and channel diagnostics in the user program of the SIMATIC S7-1200/S7-1500?
What should you watch out for when programming IEC timers in an S7-300/S7-400 and in an S7-1200/S7-1500?
Documentation for the automation system S7-1500 and the ET 200MP distributed -I/O system
More information about S7-1500


Migration from SIMATIC S5 to SIMATIC S7



Migration Guide: SIMATIC S5 to SIMATIC S7-1500
Which version of STEP 5 is compatible with which MS Windows operating system?
From S5 to S7 Converter Manual (technical status: 1997)
Configuration of S5 adapter module in an S7-400, in which 6 IMs are already configured.
How do I link an S7-400 with S5 expansion units?
STIMATIC S5 Hardware FAQs
STEP 5 FAQs
SIMATIC S5 / STEP 5 conference in the Service&Support forum
Applications and Tools with SIMATIC S5
Note: When installing STEP 7 V5.X / Prof 2010, an S5 code conversion tool is also installed


  Document with all the ID numbers of the documentation (123,8 KB)

Cable adapter
  Interface module adapter to SIMATIC S5, S7-300, S7-400 and S7-1500 (3,3 MB)


Conversion from competitor systems


Conversion Guide: Rockwell Automation PLC-5 to SIMATIC S7

Migrating Controller Software from Rockwell or Mitsubishi to Siemens


 How to integrate a modernized automation system into an existing infrastructure. (75,0 KB) 

 How to increase productivity and reduce production costs modernizing your legacy automation system. (63,8 KB) 



Training


SITRAIN:

SITRAIN – Digital Industry Academy
SITRAIN personal – Germany
SIMATIC Industrial Automation Systems


SITRAIN - UK and Ireland
SITRAIN - USA
SITRAIN - Australia
SITRAIN - Canada



Additional Information


TIA Selection Tool - Migration (Video)
Die SIMATIC S7-1500 neuester Generation von Siemens (Video)

 

Additional Keywords
Overview page, Topics page, Overview, Engineering Efficiency, Performance, Totally Integrated Automation, S5-IO adapter

Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.