×
Siemens Industry Online Support
Siemens AG
Entry ID: 83557459, Entry date: 07/09/2018
(11)
Rate

Migration of plants with SIMATIC (TIA Portal) - Controllers

  • Entry
A certain amount of know-how is required for migrating to new systems. Siemens supports you with many tools and other aids to get successfully into the TIA Portal and the new SIMATIC components.


In order to optimize the performance of a plant, it is useful to check regularly that it is state of the art. A certain amount of know-how is required for migrating to new systems. Siemens supports you with many tools and other aids to get successfully into the TIA Portal and the new SIMATIC components. Here we provide an overview of the relevant topics with links to the most important entries.






 Complete systemsController and IO
Visualization
Communication
TIA Portal

Here you have direct access to the most important technical information and solutions for controllers.

Migration tools

Migration Tool TIA Portal
In many cases a project that you wish to migrate is not on the same PG/PC as the TIA Portal. The migration tool converts the initial project into a compatible format. You can read this file into the TIA Portal and continue processing it.
TIA Portal Readiness Check Tool
The TIA Portal Readiness Check Tool delivers an easy way of checking whether the TIA Portal supports the hardware in the project.
TIA Selection Tool
The TIA Selection Tool is for selecting, configuring and ordering devices, software and licenses.

Programming languages

Programming Guidelines and Programming Styleguide for SIMATIC S7-1200 and S7-1500
SIMATIC S7-1200 / S7-1500 Comparison list for programming languages based on the international mnemonics
What should you watch out for when migrating an S7-SCL program in STEP 7 (TIA Portal)?

From STEP 7 V5.x to STEP 7 (TIA Portal)

What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)?
What are the requirements for the migration of STEP 7 V5.x projects in STEP 7 (TIA Portal)?
What are the requirements for installing STEP 7 (TIA Portal) V15.1?
How do you convert STEP 7 Professional / Basic projects in TIA Portal, which you have created with earlier versions of TIA Portal?
Why, after project migration from STEP 7 (TIA Portal) V13 SP1, does STEP 7 (TIA Portal) V14 issue the message "The data type Word of the actual parameter does not match the data type HW_IO of the formal parameter"?
Migration of a Safety Program to TIA Portal
How do you efficiently and effectively program for the S7-1200/S7-1500 in STEP 7 (TIA Portal)?
What are the differences in the keyboard operation of STEP 7 (TIA Portal) and STEP 7 V5.x?
SINAMICS G120 / G120D / G120P / G120C: Migration of a STEP 7 Classic project into a STEP 7 V12/V13 project.
Where are the standard blocks and instructions stored in STEP 7 (TIA Portal) and in V5.x (SIMATIC Manager)?
More information about S7-1200

Licenses

Which license do you need to upgrade from STEP 7 version V5.x, V11 ... V14 to the TIA Portal V15.1?
What is the difference between authorizations and license keys?

From S7-200 to S7-1200

Making the transition from S7-200 to S7-1200
What has to be considered to replace S7-200 PID applications with "PID_Compact" V2 for S7-1200?
More information about S7-1200

From S7-300/400 to S7-1500

Migration Guide: SIMATIC S7-300/400 to SIMATIC S7-1500
Migration Guide: S7-31xT to S7-1500(T)
PLC migration to S7-1500 with STEP 7 (TIA Portal)
Which entries are available in the internet concerning migration to STEP 7 (TIA Portal) and WinCC (TIA Portal)?
How can you migrate alarms in the TIA Portal from the S7-300/400 to the S7-1500?
To which differences should you pay attention in the case of retention when you migrate a GRAPH-FB in STEP 7 (TIA Portal) from S7-300/S7-400 to S7-1500?
What should you watch out for when you migrate the AG_SEND/AG_LSEND instruction from the user program of the S7-300/S7-400 in the TIA Portal to the user program of the S7-1500?
How do you implement module and channel diagnostics in the user program of the SIMATIC S7-1200/S7-1500?
What should you watch out for when programming IEC timers in an S7-300/S7-400 and in an S7-1200/S7-1500?
Documentation for the automation system S7-1500 and the ET 200MP distributed -I/O system
More information about S7-1500

Migration from SIMATIC S5 to SIMATIC S7

Migration Guide: SIMATIC S5 to SIMATIC S7-1500
Which version of STEP 5 is compatible with which MS Windows operating system?
From S5 to S7 Converter Manual (technical status: 1997)
Configuration of S5 adapter module in an S7-400, in which 6 IMs are already configured.
How do I link an S7-400 with S5 expansion units?
STIMATIC S5 Hardware FAQs
STEP 5 FAQs
SIMATIC S5 / STEP 5 conference in the Service&Support forum
Applications and Tools with SIMATIC S5
Note: When installing STEP 7 V5.X / Prof 2010, an S5 code conversion tool is also installed

  Document with all the ID numbers of the documentation (123,8 KB)

Conversion from competitor systems

Conversion Guide: Rockwell Automation PLC-5 to SIMATIC S7

Siemens Conversion Studio: Migrating Controller Software from Rockwell to Siemens

 How to integrate a modernized automation system into an existing infrastructure. (75,0 KB) 
 How to increase productivity and reduce production costs modernizing your legacy automation system. (63,8 KB) 

TIA Portal lateral entry courses

TIA-SYSUP - SIMATIC TIA Portal System-Umsteigerkurs auf SIMATIC S7-1500
VM-TIAEXP – SIMATIC S7-1500 mit TIA Portal optimal einsetzen

Cable adapter
 S5-IO adapter to SIMATIC S7-300, S7-400 and S7-1500 (1,9 MB) 


Additional Information

TIA Selection Tool - Migration (Video)
New Generation - SIMATIC S7-1500 from Siemens (video)


Additional Keywords
Overview page, Topics page, Overview, Engineering Efficiency, Performance, Totally Integrated Automation