Migration of plants with SIMATIC (TIA Portal) - Controllers
-
Entry
In order to optimize the performance of a plant, it is useful to check regularly that it is state of the art. A certain amount of know-how is required for migrating to new systems. Siemens supports you with many tools and other aids to get successfully into the TIA Portal and the new SIMATIC components. Here we provide an overview of the relevant topics with links to the most important entries.
![]() | ![]() | ![]() | ![]() | ![]() |
Complete systems | Controller and IO | Visualization | Communication | TIA Portal |
Here you have direct access to the most important technical information and solutions for controllers.
Migrationtools

Migration Tool TIA Portal In many cases a project that you wish to migrate is not on the same PG/PC as the TIA Portal. The migration tool converts the initial project into a compatible format. You can read this file into the TIA Portal and continue processing it. | |
TIA Selection Tool The TIA Selection Tool is for selecting, configuring and ordering devices, software and licenses. |
Programming languages

From STEP 7 V5.x to STEP 7 (TIA Portal)

Licenses
Which license do you need to upgrade from STEP 7 version V5.x, V11 ... V16 to the TIA Portal V17? | |
What is the difference between authorizations and license keys? |
From S7-200 to S7-1200

Making the transition from S7-200 to S7-1200 | |
What has to be considered to replace S7-200 PID applications with "PID_Compact" V2 for S7-1200? | |
More information about S7-1200 |
From S7-300/400 to S7-1500

Migration from SIMATIC S5 to SIMATIC S7

Migration Guide: SIMATIC S5 to SIMATIC S7-1500 | |
Which version of STEP 5 is compatible with which MS Windows operating system? | |
From S5 to S7 Converter Manual (technical status: 1997) | |
Configuration of S5 adapter module in an S7-400, in which 6 IMs are already configured. | |
How do I link an S7-400 with S5 expansion units? | |
STIMATIC S5 Hardware FAQs | |
STEP 5 FAQs | |
SIMATIC S5 / STEP 5 conference in the Service&Support forum | |
Applications and Tools with SIMATIC S5 Note: When installing STEP 7 V5.X / Prof 2010, an S5 code conversion tool is also installed |
Document with all the ID numbers of the documentation (123,8 KB)
Cable adapter
Interface module adapter to SIMATIC S5, S7-300, S7-400 and S7-1500 (3,3 MB)
Conversion from competitor systems

Conversion Guide: Rockwell Automation PLC-5 to SIMATIC S7 | |
Migrating Controller Software from Rockwell or Mitsubishi to Siemens |
| |
Training

SITRAIN:
SITRAIN – Digital Industry Academy | |
SITRAIN personal – Germany | |
SIMATIC Industrial Automation Systems |
SITRAIN - UK and Ireland | |
SITRAIN - USA | |
SITRAIN - Australia | |
SITRAIN - Canada |
Additional Information

TIA Selection Tool - Migration (Video) | |
Die SIMATIC S7-1500 neuester Generation von Siemens (Video) |
Additional Keywords
Overview page, Topics page, Overview, Engineering Efficiency, Performance, Totally Integrated Automation, S5-IO adapter
- German
- Spanish
- Italian
- Chinese
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry