×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 84137106, Entry date: 01/07/2019
(4)
Rate

Technical Concepts with Switchgears in Wind Turbines

  • Entry
  • Associated product(s)
Use cases show ways of using industrial controls efficiently so that communication via the PLC to the operator can ensure safe and reliable operation of the wind power plant.

Task:

Wind power plants contain - in addition to the large generator - numerous electrical components that ensure safe and reliable operation. Examples are yaw, pitch, cooling, heating components etc. Extreme electrical and mechanical requirements call for rugged and yet cost-optimized concepts. Diagnostics information must enable systematic preventive maintenance and avoid shutdowns.

 


 


Solution:

Use cases show ways of using industrial controls efficiently so that communication via the PLC to the operator can ensure safe and reliable operation of the wind power plant.

 

Downloads:

 Registrierung notwendig  Technical_Concepts_with_Switchgear_2018-09.pdf (4,2 MB)

 Registrierung notwendig  Confirmation_Contactors_3RT_for_Wind_Turbines.pdf (1,0 MB)

 Registrierung notwendig  Confirmation_Limit_Switches_3SE5.pdf (165,6 KB)

 Registrierung notwendig  Confirmation_Test_Certificate_Load_Feeders.pdf (636,8 KB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.