×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 85065340, Entry date: 12/05/2013
(0)
Rate

SinuTrain for SINUMERIK Operate 4.5 and HMI-data

  • Entry
  • Associated product(s)

Summary
SinuTrain for SINUMERIK Operate 4.5 and HMI-data

Question
How can user-specific HMI-data be used with SinuTrain for SINUMERIK Operate 4.5 and stored in the SinuTrain-machine?

Answer
Guidance how to use user-specific data in the HMI-path

Changes at the HMI-path are not supported by Siemens. But with the actual version SinuTrain for SINUMERIK Operate 4.5 it is possible to use such machine-specific data by following procedure:

  1. Start the target SinuTrain-machine.
  2. Copy all necessary data via Windows-Explorer into the respective HMI-subfolder: C:\Siemens\SinutrainOperate\04.05\hmi
  3. Shut down the SinuTrain-machine.

According to this procedure the copied data will be stored inside the SinuTrain-machine while its shut down. Other SinuTrain machine configurations will remain unchanged.

Note
Any changes in the HMI-path are on your own risk, SIEMENS will not give any support.

Additional keywords
sinutrainforoperate

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.