×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 85168215, Entry date: 04/04/2016
(4)
Rate

SINAMICS G120/G120P/G120C: Description of Free Function Blocks (FFB)

  • Entry
  • Associated product(s)
The frequency converter SINAMICS G120, G120P, G120C contain so called free function blocks, which can be used for logical and numerical operations. The instruction describes the functionality of the free function blocks and the general conditions to handle them.

Where do I find an instruction describes the functionality of the free function blocks?

see    85168215_FAQ-01X4QJPN_FFB_en.pdf (2,1 MB) 

Note

SINAMICS G120C contains free function blocks (FFB) from FW V4.7 SP6


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.