×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 85291197, Entry date: 12/19/2013
(0)
Rate

User Manual Collection – multilingual DVD with user documentation

  • Entry
  • Associated product(s)

With immediate effect, an updated DVD-ROM including the available user documentation (operating instructions, Programming Guides, Diagnostic Guides, training documentation) for the SINUMERIK 840D sl/840D/840Di/840Di sl/828D/810D/802D sl/802D/802S/802C systems is provided in German, English, French, Italian, Spanish and Chinese. Numerous other manuals are provided in additional languages.

Article number: 6FC5298-7CA00-1YG0

The User Manual Collection comprises the current documents for Software Version 4.5 SP2 for the following SINUMERIK controllers:

  • SINUMERIK 802D sl
  • SINUMERIK 828D
  • SINUMERIK 840D sl
  • SINUMERIK 840Di sl
  • SINUMERIK 802S/802C/802D
  • SINUMERIK 810D
  • SINUMERIK 840D
  • SINUMERIK 840Di

Target groups of the UserManual Collection

The User Manual Collection including the German / English / French / Italian / Spanish / Chinese documentation is intended for machine manufacturers and end customers who require the existing scope of languages of the user documentation, for example, to deliver their machines. Further, both original and pdf documents are provided for manufacturers who can use the contents from the Siemens documentation to create their own manufacturer-specific documentation. A detailed overview of the documents included is provided here:

TOC_UMC_1013.pdf ( 132 KB )

How to start the UMC

With installation:

  • Execute the "setup.msi" file and follow the Installation Wizard

Without installation:

  • Listing the documents with all their functions:

Execute the file "start_from_DVD.cmd". The Java Runtime environment is started. You can use all the functions provided by the DVD.

  • Listing the documents without further functions:

Execute the file "LIST_DOCUMENTS_ONLY.cmd". Select the requested language. You will receive a listing of all documents, the Java Runtime environment will not be started. Further functions, e.g. search options, are not provided.

More detailed information regarding the installation is provided in the file Liesmich_UMC_de.txt  ((Readme_UMC_ge.txt)). All technical manuals will also be published via the Service&Support Portal. Thus, the documents can also be used via My Documentation Manager, together with other documents dealing with automation and drives technology. The documentation is provided in the available languages on the Internet. The documentation regarding CNC controllers is provided in SIOS at: Link

System requirements

  • 2 GHz processor
  • min. 1 GByte RAM
  • Windows XP Professional SP1, SP2 or SP3
  • Windows XP Tablet PC Edition
  • Windows Vista 32: Ultimate, Business, Enterprise
  • Windows 7 Professional, Ultimate, Enterprise
  • Windows Server 2008 R2
  • Adobe Reader 9.4 (or later)
  • Internet Explorer, Version 8 (or later)
  • DVD drive
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.