Firmware Update for ET 200SP IM 155-6 PN HF
-
Entry
-
Associated product(s)
Description:
When updating the firmware, always update to the latest version available for the product and its respective article number. The previous versions of the firmware are only intended as backup to allow a downgrade to the original version. How to update the firmware is described in detail in entry ID 78646133. |
Note:
When new, replaced or upgraded I/O modules are installed, a firmware update of the IM155-6PN HF interface module with article number 6ES7155-6AU00-0CN0 to firmware version V2.1.0 or higher may also be necessary.
(Supply from Siemens stock until December 2013 inclusive).
Therefore, updating the firmware of the IM155-6PN HF interface module is generally highly recommended for modules with firmware versions < V2.1.0.
The current GSDML file for PROFINET can be downloaded here: 57138621
Overview of article numbers and firmware versions of the ET 200SP IM155-6 PN HF:
Note: Software is subject to export restrictions, download only for registered users
Article Number |
FW Version | Update with... |
---|---|---|
6ES7155-6AU00-0CN0 | ||
V4.2.4 | Third-party software - Licensing terms and copyright information You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS_V424 file. Special information for resellers The information and the license terms in the Readme_OSS_V424 file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
For Update: For STEP 7 as of Version 5.5 For STEP 7 TIA Portal | |
V4.2.3 | Third-party software - Licensing terms and copyright information You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS_V423 file. Special information for resellers The information and the license terms in the Readme_OSS_V423 file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
Backup only: For STEP 7 as of Version 5.5 For STEP 7 TIA Portal | |
V4.2.2 | Third-party software - Licensing terms and copyright information You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS_V422 file. Special information for resellers The information and the license terms in the Readme_OSS_V422 file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
Backup only: For STEP 7 as of Version 5.5 For STEP 7 TIA Portal | |
V4.2.0 | Third-party software - Licensing terms and copyright information You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS_V420 file. Special information for resellers The information and the license terms in the Readme_OSS_V420 file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
Backup only: For STEP 7 as of Version 5.5 For STEP 7 TIA Portal | |
V3.3.1 | Third-party software - Licensing terms and copyright information You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS_V331 file. Special information for resellers The information and the license terms in the Readme_OSS_V331 file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
Backup only: For STEP 7 as of Version 5.5 For STEP 7 TIA Portal | |
V3.3.0 | Backup only: For STEP 7 as of Version 5.5 For STEP 7 TIA Portal | |
V3.1.0 | Backup only: For STEP 7 as of Version 5.5 For STEP 7 TIA Portal | |
V3.0.0 | Backup only: For STEP 7 as of Version 5.5 For STEP 7 TIA Portal | |
V2.2.0 | Backup only: | |
V2.1.0 | Backup only: |
Update V4.2.4 |
Stabilization of module communication in conjunction with AI Energy Meter 480V RC/CT HF and I/O modules with cyclic user data larger than 32 bytes.
Update V4.2.3 |
Increase the ruggedness of network communication with uninterrupted continuous operation of more than 497 days.
To support the check whether the system configuration used in the individual case is affected, and if any measures must be adopted, contact the Technical Support (Service Request required).
Update V4.2.2 |
Improved diagnostic behavior in case of failed PROFINET connection in conjunction with empty locations and PotDis modules
Update V4.2.0 |
Firmware revision as part of product maintenance
Functional expansion:
- Support of system redundancy S2 on CPU S7-1500R/H
- Support of clock synchronization in conjunction with Shared Device
- Support of the tool changer as docking station
- Improved IT security behavior (correction for SSA-346262 und SSA-293562),
see Siemens ProductCERT and Siemens CERT
Update V3.3.1 |
The Firmware V3.3.1 comprises the following improvements:
- Correction of a sporadically pending parameterization error diagnostics with S2 system redundancy in combination with a station stop
- Improvement of the behavior shown by the Profinet user data companion when inserting and removing peripheral modules
- The behavior shown when performing a network scan using the Proneta tool has been improved
Update V3.3.0 |
The following new functions have been implemented:
- Support of parallel submodules
- Support for maintenance diagnostics
- Changeover to extended channel diagnostics
- Support for glass-fiber BusAdapters (LC)
Update V3.1.0 |
The following new function was implemented:
- Support of electronic modules with up to 288 Byte user data
Update V3.0.0 |
The following functions are supported with the new firmware version:
- Station expansion with ET 200AL IP67 I/O line over ET connection
- Support of the NAP S2 system redundancy
- Configuration of Shared Device and MSI/MSO by means of MDD (TIA-Portal)
- PROFINET V2.3 support.
Update V2.2.0 |
The following new functions have been implemented:
- Support module-internal Shared Input / Shared Output (MSI/MSO)
- Configuration with TIA Portal V13
- Configuration with Step7 V5.5 SP3 and HSP250/255
Update V2.1.0 |
The following new functions have been implemented:
- Support of the isochronous mode of I/O modules
- Support of the operation of failsafe electronic modules
- Configuration with TIA Portal V12.01and HSP0058
- Configuration with Step7 V5.5 SP3 and HSP233
The following change has been implemented:
The scalable I/O systems provides the possibility of implementing new functions retrospectively via a firmware update for existing I/O modules.
If these firmware extensions make configuration-relevant changes necessary, the firmware of the IM155-6PN HF interface module (6ES7 155-6AU00-0CN0) also needs to be updated to ensure compatibility regarding the replacement of I/O modules updated in this way.
The firmware update is highly recommended.
- German
- French
- Spanish
- Chinese
- Italian
Entry belongs to product tree folder(s):
- Automation Technology Automation Systems Industrial Automation Systems SIMATIC I/O systems ET 200 systems for the cabinet ET 200SP Interface Modules IM 155-6
- Automation Technology Products for specific requirements Automatision technology for extreme conditions SIPLUS extreme Industrial Automation Systems SIPLUS IO systems SIPLUS ET 200 Systems for the Cabinet ET 200SP SIPLUS Interface Modules without CPU
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry