×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 86296587, Entry date: 02/14/2014
(0)
Rate

Why are the menus grayed out in the WinCC User Archive Editor and why is editing not possible?

  • Entry
  • Associated product(s)

Description
In a server-client configuration it might happen that you cannot edit in the WinCC User Archive Editor. In this case the menus are displayed in gray.


Fig. 01

Since you can configure also from a client in a server-client configuration, WinCC has a safety mechanism that prevents multiple persons from making changes in the WinCC User Archives at the same time. For this, a "UAEditor.loc" file is created in the project directory when the User Archive Editor opens and deleted when editing has finished.

Instructions
Under certain circumstances it might happen that this file is not deleted in the project directory after editing has finished. This then prevents further processing even though nobody else is making changes. In this case you navigate in Windows Explorer to the project folder and delete the "UAEditor.Loc" file manually.


Fig. 02

Note
This behavior can also occur in other editors. Also refer to Entry ID 492977.

Additional Keywords
User archive

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Hinweis: Das Feedback bezieht sich immer auf den vorliegenden Beitrag. Ihre Nachricht wird an die Redakteure im Online Support gesendet. In einigen Tagen erhalten Sie von uns eine Antwort, wenn Ihr Feedback das erfordert. Ist für uns alles klar, werden wir Ihnen nicht mehr antworten.