×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 8722972, Entry date: 09/05/2001
(0)
Rate

The "PC/PPI Cable (PPI)" interface cannot be installed in "Set PG/PC interface"

  • Entry
  • Associated product(s)

QUESTION:
Why can't I install the "PC/PPI Cable (PPI)" interface in "Set PG/PC interface"?

ANSWER:
You have installed STEP 7 V5.1 / SP2 alongside an existing installation of STEP 7-Micro/Win32. Now you want to add the "PC/PPI Cable (PPI)" interface via "Start > Settings > Control Panel > Set PG/PC interface > Install". But it is not possible to insert the interface.

Remedy:
Install STEP 7-Micro/Win32 V3.1 with SP2.

Keywords:
Interface parameterization

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.