Entry type:
Download
Entry ID:
8806155,
Entry date:
09/26/2001
Rate
Service Tools TELEMASTER / Service-IBS V5.0.1
-
Entry
-
Associated product(s)
DESCRIPTION:
For simple start-up of STEP7/CFC/D7-SYS projects you can use the service tools "TELEMASTER" and "Service-IBS".
You only need a standard windows95/98 PC for the both DOS utilities. A STEP7/CFC/D7-SYS installation is not nescessary.
For simple remote diagnostics a PC with installed "TELEMASTER" software is nescessary on the operator side and on the plant side.
Running notes
- Using with DOS and Windows 95/98
Service-IBS/TELEMASTER are originally DOS programs, which are also running with Windows 95/98. The highest operating speed can be achieved when running with DOS. - Using with Windows NT
IBS/TELEMASTER are not released for Windows NT because correct function is depending on type of the PC/notebook which is used! If it is intended to use IBS/TELEMASTER with Windows NT, the user has to test them with the PC/notebook used. Other Window programs should not be active in that case. - Working together with STEP 7/CFC
If IBS/TELEMASTER should be used together with STEP 7/CFC on the same PC following has to be considered:
a) Operating of IBS/TELEMASTER and CFC-testmode simultaneously in their related windows and working on the same COM serial interface of the PC is not possible!
b) Starting the CFC-testmodus after closing IBS/TELEMASTER at the same COM serial interface is possible. If the starting sequence is the other way round, i.e. if the IBS/TELEMASTER has to be started after having left the CFC-testmodus, the PC has to be reseted and booted again before starting the IBS/TELEMASTER. - Application module FM 458
IBS/TELEMASTER are not released for the application module FM 458. If it is intended to use IBS/TELEMASTER with the application module FM 458, the user has to test them.
Start-up Tool Service-IBS V5.0.1 ibs501.zip ( 804 KB ) ( 804 KB )
Remote Diagnostics and Start-up Tool TELEMASTER V5.0.1 tele501.zip ( 804 KB ) ( 804 KB )
Keywords
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Also available in the following languages:
- German
- French
- Italian
- Chinese
Rate entry
Requests and feedback
What do you want to do?
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry
Support to the statistics
With this function the IDs found are listed according to number (format .txt).
Copy URL
mySupport Cockpit
Product information