×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 88581846, Entry date: 08/06/2014
(0)
Rate

SINUMERIK 840D sl release for sale and delivery CNC-SW 4.5 SP3

  • Entry
  • Associated product(s)

[Update 05.08.2014]

SINUMERIK 840D sl CNC software 4.5 SP3 has been released for sale and delivery. Please note that the "SINUMERIK Operate /NCU" option also has to be ordered and licensed when ordering CNC software 4.x since October 1, 2013 for using SINUMERIK Operate in the NCU.

[Update 05.08.2014]

New options and functional improvements

  • Operation of the ET 200 SP failsafe modules on SINUMERIK 840 D sl. (For further details see 87603038.)
  • Option 6FC5800-0AP67-0YB0 (P67): SINUMERIK INTEGRATE ACCESS MYMACHINE /OPC UA.
    The software option SINUMERIK Integrate Access MyMachine /OPC UA enables the communication channel for the OPC UA Server on the SINUMERIK PCU or on the SINUMERIK NCU. The OPC UA Data Access method permits the reading and writing of CNC and PLC tags. OPC Unified Architecture OPC UA is a standardized, industrial communication protocol for providing access to control data, e.g. by control systems
  • By using the "SINUMERIK Operate /NCU" option (6FC5800-0AS00-0YB0 / S00) SINUMERIK Operate is activated in the CNC software for the NCU. When SINUMERIK Operate is used in the CNC software version 4.x, the "SINUMERIK Operate /NCU" option must also be ordered and licensed..
    Caution:

    SINUMERIK Operate for NCU has had its own license since October 1, 2013. For this reason, it has been necessary since October 1, 2013 to order the "SINUMERIK Operate /NCU" option, if SINUMERIK Operate is used or activated in the NCU for SINUMERIK 840D sl for CNC software release 4.x or higher. Please take this into account when placing your orders

Additional functional improvements

  • see upgrade instructions

Released components

Article number

Designation

CNC SOFTWARE from 4.x  on CF card with license, current software version
6FC5851-1YG00-0YA0 CNC-SOFTWARE 31-3 WITH SINUMERIK OPERATE, EXPORT
6FC5851-1XG00-0YA0 CNC-SOFTWARE 31-3 WITH SINUMERIK OPERATE
CNC SOFTWARE from 4.x  on CF card without license, current software version
6FC5851-1YG00-0YA8 CNC-SOFTWARE 31-3 WITH SINUMERIK OPERATE, EXPORT
6FC5851-1XG00-0YA8 CNC-SOFTWARE 31-3 WITH SINUMERIK OPERATE
CNC SOFTWARE 4.5 SP3  on CF card with license  (04.05.03.00.018)
6FC5851-1YG41-3YA0 CNC-SOFTWARE 31-3 WITH SINUMERIK OPERATE, EXPORT
6FC5851-1XG41-3YA0 CNC-SOFTWARE 31-3 WITH SINUMERIK OPERATE
CNC SOFTWARE 4.5 SP3  on CF card without license  (04.05.03.00.018)
6FC5851-1YG41-3YA8 CNC-SOFTWARE 31-3 WITH SINUMERIK OPERATE, EXPORT
6FC5851-1XG41-3YA8 CNC-SOFTWARE 31-3 WITH SINUMERIK OPERATE

Notes

The order number includes consecutive numbering; this means that the software version can no longer be directly read. Up till now, the following software releases for SW 4.xx have been launched. When ordering current software, the new release 4.5 SP3 will be supplied.

Software version Article number
SW 4.4 SP1 6FC5851-..G40-1YA0
SW 4.4 SP2 6FC5851-..G40-2YA0
SW 4.4 SP2 HF2 6FC5851-..G40-3YA0
SW 4.4 SP3 6FC5851-..G40-4YA0
SW 4.5 SP1 6FC5851-..G41-1YA0
SW 4.5 SP2 6FC5851-..G41-2YA0
SW 4.5 SP3 6FC5851-..G41-3YA_

Upgrade instructions/supplementary conditions/compatibilities

Upgrade instructions

General conditions

For SINUMERIK 840D sl, the Safety Integrated functional area will be innovated over the medium and long terms. As a result of preparatory measures (changing the PLC operating system), this means that from software release 4.4 in the hardware configurator, the PLC must be addressed as F-PLC. However, the F functionality of the integrated PLC will not be available in this software release, but only in phases in future software releases.

Compatibilities regarding SW 4.5 SP3

Article number

Designation

6FC5860-1YC41-3YA0 SINUMERIK Operate 4.5 SP3
6FC5860-0YC40-0YA8 SINUMERIK Operate 4.5 SP2 language extensions
6FC5860-7YC10-1YA0 SINUMERIK Integrate Access MyMachine/P2P(MCIS RCS COMMANDER); FOR PC/PG; SOFTWARE 2.6
6FC5250-7AY00-7AG0 SINUCOM COMMISSIONING/SERVICE TOOL SW 7.7
6FC5252-5AY01-5AG0 STEP 7 for SINUMERIK 5.5 or higher
6SL3072-0AA00-0AG0 STARTER COMMISSIONING TOOL FOR SINAMICS AND MICROMASTER VERSION V4.3.2

For further information regarding SINUMERIK Operate 4.5 SP3, see 88579123.

For more detailed information, please contact your local Siemens office.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.