×
Siemens Industry Online Support
Siemens AG
Тип сообщения: Часто задаваемые вопросы, ID сообщения: 8861819, Дата сообщения: 25.06.2013
(41)
Оценить

How do you disable the message "Please reboot before installing any more programs"?

  • Сообщение
  • Относится к продукту(ам)
You can solve the problems by making changes in the Registry.

Instructions
The Microsoft Windows operating system has registered one or more write-protected files for deleting or renaming. This is the cause of the behavior described above and cannot be influenced by the relevant software.

If you get the error message described above after installing the software, although you have rebooted your PC, as a remedy we recommend the procedure below.

Note
In general, no warranty can be given for direct changes made in the Registry because this is entirely the responsibility of the user. In any event, you are advised to make a backup of the Registry before undertaking the actions described here. Furthermore, these settings are computer-specific. This means that when you copy the project to another computer, you must make the settings again.
 

No.Procedure
1Open the Registry editor by starting the "regedit.exe" file in this path: "C:\Windows". Check whether the value "PendingFileRenameOperations" is in the path "HKEY_LOCAL_MACHINE\System\CurrentControlSet\Control\Session Manager".




Fig. 1
 
2

In the right window double-click the value "PendingFileRenameOperations" to open the editor for multiple character strings.


Fig. 2

The entries in this editor (Fig. 02) are to be interpreted as follows: Windows generates two lines for each file concerned.

  • Case a
    If the second of the two lines is empty, it means that the file has been registered to be deleted. In this example, the Au_.exe file in the directory
    "C:\Users\z002tbus\AppData\Local\Temp\~nsu.tmp" would be deleted via the Windows Explorer.
  • Case b
    If there is an entry in the second of the two lines, that is the new name for the file in line 1. In this example the file nsu.tmp in the directory
    "C:\Users\z002tbus\AppData\Local\Temp" would be renamed via the Windows Explorer.


Note
The abovementioned files and paths to be deleted are just an example. Here you delete the paths and files that are displayed in the editor on your computer.
 

3After completing the steps described above you delete the value "PendingFileRenameOperations" in the Registry code "HKEY_LOCAL_MACHINE\System\CurrentControlSet\Control\Session Manager\ " via pop-menu (right-click).

Now you can install more programs without having to restart the computer again.
 

Notes on installing S7 Technology
If, when you are installing S7 Technology, the same thing happens as described above, check the entry in the following code in the Windows registry: "HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\RunOnce"

If a value is entered here, delete it. Restart your computer and then try the installation again.

Note for HP Notebooks
If the recommendations above (Points 1 to 4) do not help with HP Notebooks (NC6120, for example), we recommend updating the WLAN driver or removing the HP Wireless Wizard from the Registry.


Указания по безопасности
Для того чтобы обеспечить кибербезопасность установок, систем, машин и сетей, необходимо внедрить и постоянно поддерживать в работоспособнобном состоянии комплексную концепцию по обеспечению секретности на промышленных объектах, которая соответствует современному техническому уровню. Продукция и решения Сименс являются лишь частью такой концепции. Более подробно о мерах обеспечения секретности на промышленных объектах можно узнать на
http://www.siemens.com/industrialsecurity.
Поддержка статистики
Данная функция позволяет выдавать идентификаторы (ID) результата поиска согласно желаемому количеству (формат .txt)

Генерировать список
Копировать URL
View this page in new design
Панель управления mySupport
Ссылки по теме
    Тематические страницы для данных записей