×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 8861819, Entry date: 09/11/2019
(107)
Rate

How do you disable the message "Please reboot before installing any more programs"?

  • Entry
  • Associated product(s)
You can solve the problems by making changes in the Registry.

Description
The Microsoft Windows operating system has registered one or more write-protected files for deleting or renaming. This is the cause of the behavior described above and cannot be influenced by the relevant software.

If you get the error message described above after installing the software, although you have rebooted your PC, as a remedy we recommend the procedure below.

Note
In general, no warranty can be given for direct changes made in the Registry because this is entirely the responsibility of the user. In any event, you are advised to make a backup of the Registry before undertaking the actions described here. Furthermore, these settings are computer-specific. This means that when you copy the project to another computer, you must make the settings again.

Instructions

  1. Open the Registry Editor by simultaneously pressing the "[Windows] + [R]" buttons.
  2. Enter "regedit" in the input field and click OK.
  3. In the Registry Editor you navigate to the path "HKEY_LOCAL_MACHINE\System\CurrentControlSet\Control\Session Manager".
  4. Check whether the value name "PendingFileRenameOperations" is in the path.
     

    Fig. 1
     
  5. Delete "PendingFileRenameOperations" and then close the Registry editor.
  6. Then immediately start the program installation without prior restarting.

Note on installing S7 Technology
If, when you are installing S7 Technology, the same thing happens as described above, also check the entry in the following code in the Windows Registry: "HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\RunOnce"
If, after a reboot, a value is entered here, delete it. Restart your computer and then try the installation again.

Note for HP Notebooks
If the instructions above do not help with HP Notebooks (NC6120, for example), we recommend updating the WLAN driver or removing the HP Wireless Wizard from the Registry.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.