×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 89255803, Entry date: 03/03/2014
(2)
Rate

Update 1 for SIMATIC powerrate V4.0 SP2

  • Entry
  • Associated product(s)

DESCRIPTION:
Download of Update 1 for
SIMATIC powerrate V4.0 SP2

Installation Prerequisite:

  • SIMATIC powerrate V4.0 SP2


Information about Update 1

Please observe the installation and usage instructions in the following PDF file:

simatic_powerate_V402_update_01_readme_de-DE_en-US.pdf ( 49 KB )

Note:
Beside several improvements, the Update also contains the following innovated S7 Blocks:

  • PRx_BIN_ACQ

  • PRx_SUM

  • PRE_AR_DATA

  • PRE_AR_SND

After the installation of the update, these Blocks must be updated also in your S7 User Program. You can find a detailed description in the chapter 2.7 ‘How to perform an upgrade installation from SIMATIC powerrate’ in the Release Notes von SIMATIC powerrate V4.0 SP2 (85193670).


Download Update 1 for SIMATIC powerrate V4.0 SP2

Powerrate_V40_SP2_Upd1.exe ( 59518 KB )


Installation of Update

Exit all applications (e.g. MS Excel etc.) before you start setup.


Running the installation

The setup program will guide you through the entire installation.
Depending on the system configuration, a revoot may be required after installation.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.