×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 89332241, Entry date: 10/23/2018
(2)
Rate

Integration of Advanced Process Graphics in SIMATIC PCS 7

  • Entry
  • Associated product(s)
New HMI concepts such as Advanced Process Graphics (APG) are the key to task-specific or situation-specific decision-making criteria. APG is a visualization concept in which the plant operator and his tasks are the central focus.

The main application of APG is the visualization of plant sections in overview displays as well as the display of the overall process status. APG offloads plant operators and ensures that, despite increasing complexity and the expansion of operator tasks, the plant operator's work becomes simpler and more efficient.

This application example describes the use of APG to improve process visualization using the "Polymerization Reactor" unit template as an example. Process pictures for Levels 1 and 2 of the topology and task-oriented plant hierarchy are created for this purpose.

  • Level 1 process picture (Orientation and Navigation)
    A process picture with a compressed representation of the main driving parameters is created for monitoring the process-related parameters of the overall system. This allows the overall context to be quickly detected and impressed as a pattern.

     
     
  • Level 2 process picture (Operation and Monitoring)
    A process picture is created for monitoring the process-related parameters of the reactor and also for operator control, which schematically represents the most important process values and control of the reactor. This representation has the advantage that large volumes of data can be combined to form a compressed and clear display of information.

     

Advantages
One of the most important advantages of APG is that deviations from normal operation (working range) are easily detected due to the schematic representation before limiting values are breached or alarms are triggered. On the other hand, with technology-oriented visualization, recognition of the plant status is only possible as a result of the plant operator's know-how.
Further advantages:

  • Compact, simplified presentation in overview screens
  • Efficient execution of operating tasks by means of situation and task-specific process views
  • Focusing the attention for short reaction times
  • Improvement of the process comprehension

Video


Introduction to process visualization with Advanced Process Graphics

Validity

  • SIMATIC PCS 7 V9.0 SP1 with APG V9.0 SP1
  • SIMATIC PCS 7 V8.1 with APG V8.1
  • SIMATIC PCS 7 V8.0 with APG V8.0

Documentation for PCS 7 V9.0 SP1
  Integration of Advanced Process Graphics in SIMATIC PCS 7 (5,8 MB)

Documentation for PCS 7 V8.1 and PCS 7 V8.0
  Integration of Advanced Process Graphics in SIMATIC PCS 7 ( (5,3 MB)

PCS 7 sample project with APG
PCS 7 Unit Template "Polymerization Reactor" using the example of the chemical industry

Further information
APG product and ordering information

Last change
Update for SIMATIC PCS 7 V9.0 SP1 with APG V9.0 SP1, new chapter for new APG-Function added

Additional keywords
Visualization, OS runtime, E-Learning, Tutorial, Teaser, Webcast, Multimedia-based demonstration system, MMDS, Film, Screencast, video,

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.