×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 89373182, Entry date: 03/07/2014
(0)
Rate

SINUMERIK Integrate Package SW4.0 SP3

  • Entry
  • Associated product(s)

Virus message output when installing SINUMERIK Integrate for Production V4.0 SP3
This is a false message !

Due to new virus patterns installed in the virus scanners, a virus message is output when installing SINUMERIK Integrate for Production V4.0 SP3. However, this is a false message.

The apparent virus reported refers to the "Setup.exe".

Example:

This concerns all the old MDA and AMP versions, that means, also the MDA 2.2 and SINUMERIK Integrate for Production V4.0 SP3 versions which have been released and are currently available.
You can ignore this virus message.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit