×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 89770537, Entry date: 04/22/2014
(2)
Rate

SINUMERIK 840D sl: Resuming to drill a pattern of holes (Block Search)

  • Entry
  • Associated product(s)

Description
The design of a program, for the drilling of a pattern of holes, is easily possible with SINUMERIK Operate. During the machining, however, the program could be reset because of an error or because of a manual reset (e.g. when boring deep holes). How can the program being restarted, after the reset, from the last drilled position and not from the beginning? How can the manufacturer implement this resuming? “Block Search” is provided in SINUMERIK Operate as a standard. When the program has been resetted, the softkey “Block search” can be pressed. SINUMERIK Operate lets then to choose, how to prepare the program for the resuming:

 

Downloads

Content of Downloads

download

Documentation 89770537_Resuming-To-Drill-A-Pattern-Of-Holes-Block-Search.pdf ( 2593 KB )

Last Changes
First Edition

Additional search terms
motioncontrol_cnc_applications

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.