×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 90063835, Entry date: 03/25/2014
(0)
Rate

Which firewall settings do you have to make for smooth operation of the SINEMA Server V12?

  • Entry
  • Associated product(s)

Description
It might happen that the SINEMA Server does not start and issues an error message or devices are not recognized in the network. The cause for this might be an incorrect firewall configuration.

Firewall settings
By default you must enable the ports in the list below. However, most ports can be changed through the Windows operating system or in the SINEMA Server.

Firewall between SINEMA Server and the network:

  • Port 80, TCP, http
  • Port 443, TCP, https
  • Port 161, UDP, SNMP
  • Port 162, UDP, SNMP Traps
  • Port 25, TCP, SMTP

Firewall between SINEMA Server and a client:

  • Port 80, TCP, http
  • Port 443, TCP, https

Firewall between SINEMA Server and an HMI/OPC client:

  • Port 80, TCP, http
  • Port 443, TCP, https
  • Port 4840, TCP, OPC UA

Note
If you change the ports (for example, http from Port 80 to Port 8080) in the SINEMA Server, then you must also change your firewall rules.

Security notes
Siemens offers products and solutions with industrial security functions which support the secure operation of plants, solutions, machines, devices and/or networks. They are important components in a comprehensive industrial security concept. The Siemens products and solutions continue to be developed under this aspect. Siemens recommends that you keep yourself regularly informed about product updates.
For the safe operation of Siemens products and solutions it is necessary to take appropriate security measures (cell protection concept, for example) and to integrate each component in an overall industrial security concept which is state of the art. This should also cover the third-party products used. Additional information about industrial security is available at:
http://www.siemens.com/industrialsecurity.
In order to keep yourself informed about product updates, we recommend subscribing to our product-specific newsletter. Additional information about this is available at
http://support.automation.siemens.com.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.