×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 90161753, Entry date: 04/09/2014
(2)
Rate

SINUMERIK 810D/840D: Reading out the drive data via the NCVAR selector

  • Entry
  • Associated product(s)

Question
What is important when reading out drive data via the NCVAR selector?

Answer
See the following table for the requirements for reading out drive data.
 

Enabl Option
General NC enable Evaluation of internal drive variables
(order number 6FC5251-0AB17-0AA0)
Axis-specific enable Detection of additional drive actual values

With MD36730 $MA_DRIVE_SIGNAL_TRACKING = 1, acquisition of the following drive actual values is activated (if they are provided by the drive):

  • $AA_LOAD drive load
  • $AA_POWER drive active power
  • $AA_TORQUE drive torque setpoint
  • $AA_CURR smoothed current actual value (quadrature-axis current) of the drive

During operation of the NC control, different conditions arise. Similarly, system-specific data can change during operation. These data are termed status data as opposed to system data. A distinction is made between

  • NCK-specific status data
  • Mode-group-specific status data
  • Channel-specific status data
  • Drive-specific status data (FDD)
  • Drive-specific status data (MSD)

You will find drive-specific status data feed drive (FDD) in area V, block S of the NCVAR selector.

Caution
No cyclic service must be set up on variables in this block. Only individual variable accesses are permitted.

You will find drive-specific status data main spindle drive (MSD) in area H, block S of the NCVAR selector.

Note
Addressing of the H-S block is not possible in MMC100/EBF/OP 030.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit