×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 90277865, Entry date: 08/19/2014
(0)
Rate

SINUMERIK: 5-axis circular pocket-hole milling

  • Entry
  • Associated product(s)

Description
With multiaxis machining, the main objectives are to achieve perfect surface quality, precision, and speed without any need for remachining (reworking). Specifically in tool and mold making as well as in the aerospace domain, complex surface geometries must be machined with a high degree of precision in a short time. A machine tool is required, which in addition to linear axes X, Y and Z, has at least two additional rotary axes (rotation around the linear axes). The rotary axes must be able to be simultaneously controlled.
A hole is to be milled in a cylinder using 5-axis transformation. Drilling motion is helical, the milling tool position is positioned at a specific angle and tilted backward when milling. The TRAORI function with orientation vectors A3, B3, C3 is used in order that the milling tool can be optimally used, and/or the diameter of the milling tool (for generally used milling tool sizes) is independent of the hole diameter. The 5-axis helical solution can be applied for holes and circular pockets.

Downloads

Content of downloads

Download

Documentation 90277865_5-Axis_Circular_Pocket-hole_Milling.pdf ( 2346 KB )
Programs 90277865_NC_Programs.zip ( 963 KB )

Last Changes
First Edition

Additional search terms
motioncontrol_cnc_applications

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.