×
Siemens Industry Online Support
Siemens AG
文档类型 应用与工具 文档编号 90468030, 文档发布日期 2017年1月12日
(3)
评估

SINAMICS V: Speed Control of a V20 with S7-1500 and ET 200SP via USS® Protocol, with HMI Connection

  • 文档
  • 涉及产品
Speed Control of a SINAMICS V20 with SIMATIC S7-1500 and SIMATIC ET 200SP via USS® Protocol
SINAMICS V20
The SINAMICS V20 is compactly designed and can be adjusted individually to the requirements of the application as well as the demands of the users via various options (such as external BOP, connecting cables, filters, brake resistors, shielding, ...). The compact and robust devices are tailored for the operation of pumps, fans, compressors and conveyor systems, as well as for simple drive tasks in the processing and production industry.

Task
Drive connection by means of USS® protocol

  • Cyclic write/read access of a SIMATIC S7-1200 to selected SINAMICS V20 process/control data whose transmission is supported by a STEP7 system instruction.
  • Acyclic write/read access of a SIMATIC S7-1200 to selected SINAMICS V20 data that is exchanged via parameter accesses via STEP7 system instruction.
  • Distributed connection of the drives via SIMATIC ET 200SP.

The above tasks are supported by a KTP600 operator panel so that you can control the drives via their control word bits, specify speed setpoint values, monitor status bits and read out actual speed values. You can furthermore conveniently read out and change a number of inverter data and parameters.

Solution
The SINAMICS V20 drives are connected to the SIMATIC controller  via decentralized ET 200SP stations. Into the ET 200SP PtP, communication modules can be plugged, where each of them can serve up to 16 SINAMICS V20 via the USS® bus. The user function blocks work with the STEP7 system instructions USS_Port_Scan, USS_Drive_Control, USS_Read_Param and USS_Write_Param. The operater panel KTP600 can be simulated on the TIA portal, so the hardware concerned is not absolutely necessary. The application example supports a hardware configuration with 1 ET 200SP, which contains 1 PtP module. This allows you to connect up to 16 drives. How to expand the configuration to more peripheral stations with more PtP modules see the application description.


Downloads

  Documentation (2,1 MB) 

 Registrierung notwendig  STEP 7 Project for TIA V15 (1,3 MB)
 Registrierung notwendig  STEP 7 Library (only user FBs) for TIA V15 (808,7 KB)

 Registrierung notwendig  STEP 7 Project for TIA V14 (1,3 MB)
 Registrierung notwendig  STEP 7 Library (only user FBs) for TIA V14 (499,6 KB)

 Registrierung notwendig  STEP 7 Project for TIA V13 update 1 (3,8 MB)
 Registrierung notwendig  STEP 7 Library (only user FBs) for TIA V13 update 1 (941,5 KB)

 Registrierung notwendig  STEP 7 Project for TIA V12 SP1 update 4 (4,0 MB)
 Registrierung notwendig  STEP 7 Library (only user FBs) for TIA V12 SP1 update 4 (985,6 KB)

USS protocol for retrofit in machine and plant engineering
The use of the USS protocol for the exchange of data between a SIMATIC S7-1200/1500 can be used very sensibly for the retrofit of machines and plants.
There is often the wish to keep the existing drive landscape, consisting of MICROMASTER 4xx and MASTERDRIVES drives and only to update the automation system. This will be particularly the case for expanded machines and plants in order to limit the investment volume.

Additional Keywords
motioncontrol_apc_applications

Last Changes  
corrected wiring in documentation
Added projects for TIA Portal V15


安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.