×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 90472232, Entry date: 01/26/2017
(4)
Rate

RFID connection via ET 200 serial communication modules

  • Entry
  • Associated product(s)
The RFID readers of SIMATIC Ident shall be connected to a SIMATIC S7-CPU via distributed I/O (ET 200MP/200SP/200S) and operated in order to realize cost-efficient usage of the readers.

Solution
In this application example, block libraries are supplied which enable operating RFID readers (RF200/RF300/RF600) via distributed I/O without RFID communication modules. Furthermore, you will find a practical application example which discusses the handling of the library blocks in greater detail.
You can use all PROFINET-capable CPUs from the SIMATIC S7-300/S7-400/S7-1500. The readers are connected serially to the distributed I/Os (via the respective communication modules).

The following basic functions are realized by the blocks of the library:

  • RESET (resets the RFID reader)
  • READ (reads from transponders in the Reader field)
  • WRITE (writes to transponders in the Reader field)
  • INIT (initiates transponders in the Reader field)
  • ANT (switches the antennas of the readers on/off)

The following figure shows the possible hardware combinations covered with the library blocks:


Note: The library can be used with a CM PtP connected to an ET 200MP as well as with a CM PtP connected directly to an S7-1500.

Downloads for STEP 7 V5.5
  Documentation of the block library for S7-300/S7-400 and ET 200MP/200SP/200S (862,9 KB) 
 Registrierung notwendig  Block library for S7-300/S7-400 and ET 200MP/200SP/200S (172,1 KB) 

Downloads for STEP 7 V13
  Documentation of the block library for S7-300/S7-400/S7-1500 and ET 200MP/200SP/200S (932,4 KB) 
 Registrierung notwendig  Block library for S7-300/S7-400/S7-1500 and ET 200MP/200SP/200S (8,5 MB) 
  Documentation of the example project with S7-1500 and ET 200SP (1,3 MB)
 Registrierung notwendig  Example project with S7-1500 and ET 200SP (8,5 MB) 

Last Changes
Bug fix



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.