×
Siemens Industry Online Support
Siemens AG
文档类型 应用实例与扩展工具 文档编号 90529409, 文档发布日期 2020年10月7日
(5)
评估

Application of the device-specific blocks for IO-Link

  • 文档
  • 涉及产品
This application uses a concrete example to illustrate the simple connection of Siemens IO-Link devices to a SIMATIC S7-CPU using the Library for IO-Link

Systematic diagnostic concepts and efficient handling of parameter data are demanded in automation technology on all levels. It is imperative here that sensors and switching devices are integrated into the automation compound.
Communication IO-Link offers new possibilities through intelligent connection of sensors and switching devices to the control level. Main topics are switching, protecting and monitoring on field level.
The IO-Link system consists of an IO-Link master and one or several IO-Link devices (sensors or actuators). The IO-Link master works as interface for superimposed control and controls the communication with the connected IO-Link devices.

The application illustrates the usage of the Library for IO-Link (LIOLink) using three scenarios with SIRIUS IO-Link components. The following scenarios are realized for various IO-Link master and PNIO controllers:

  1. Simple reading and writing of data records.
  2. Generating a program alarm using a diagnostic data record.
  3. Save and restore the configuration parameters.

The operation is handled via a WinCC user interface.

Hardware setup
The following scheme shows the hardware setup of the application: 


Hardware setup 

Downloads
  Documentation (1,4 MB)
 Registrierung notwendig  Example project for TIA Portal V16 (9,7 MB)

The library of this entry was integrated entirely into the Library for IO-Link (LIOLink). You will find the library in the entry 82981502.

The last release of the library of this entry prior to the integration into the Library for IO-Link is available to download below. Note that this release will no longer be supported.

Archive
 Registrierung notwendig  Example project for STEP 7 V13 SP1 (12,3 MB)
 Registrierung notwendig  Library for STEP 7 V13 SP1 (V2.1) (5,2 MB)
 Registrierung notwendig  Library for STEP 7 V5.5 (V2.1) (1,2 MB)

Further information
Library for IO-Link (LIOLink)
S7-PCT for IO-Link Master


Last Changes

  • Integration of the library of this entry into the Library for IO-Link (LIOLink)
  • Update of the project to the newest version of the blocks of the Library for IO-Link (LIOLink)
安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
评估文档
无评估
请求和反馈
您想要做什么?
注意:反馈总是与当前的条目/产品相关。您的消息将被转发给我们在线支持团队的技术编辑们。如果我们需要就您的反馈提供答复,您将在几天内收到答复。如果没有其它问题,您将不会收到答复。