×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 90924135, Entry date: 05/12/2014
(5)
Rate

Detecting PROFINET Topologies and Activating of IO-Devices

  • Entry
  • Associated product(s)
Task In series machine building and in all areas where machine configurations change frequently, the user program requires a high degree of flexibility. Program modifications during operation or for different types of series machines are expensive and require specific expertise. Programming the a...

Task
In series machine building and in all areas where machine configurations change frequently, the user program requires a high degree of flexibility. Program modifications during operation or for different types of series machines are expensive and require specific expertise. Programming the activation / deactivation of individual IO devices, for example using a panel, involves costs both for the customer and for the configuration. The best solution in such a case is that the plant automatically detects which IO devices and therefore which machine units are connected to the central production unit (CPU). Based on the detected IO devices, these devices are activated and the suitable user program is called for configuring.


 


Solution
With its standardized data records, PROFINET provides the option to retrieve information about the accessible IO devices of a plant. This application uses this option:
The detected hardware configuration / accessible IO devices are activated and the user program is executed based on the detected configuration. The read out information is compared to a database that has previously been created.
This example shows the basic procedure using an S7-1500 as the PROFINET IO controller and three PROFINET IO devices (ET200 MP and ET200SP).

The shown configuration represents the maximum configuration used in the application. However, it can be expanded as required (within the scope of the quantity framework of the CPU). To do so, only one data block needs to be changed.

Among other things, the application contains solutions to the following tasks:

  • Reading device names out of IO devices
  • Activating / deactivating IO devices

Advantages

  • Easy installation and startup as only one user program is necessary.
  • No manual switching between different configurations of a machine, the configuration is detected automatically. This results in low technical requirements for the operating staff.

Downloads

Content of Downloads

Download

Documentation 
Dynamic PROFINET Topologies
90924135_Dyn_PN_Topo_v10_en.pdf ( 942 KB )
Code  90924135_Dyn_PN-Topo_CODE_v10_TIAP_V12_1.zip ( 2126 KB )


To stay informed about product updates as they occur, sign up for a product-specific newsletter. For more information, visit
http://support.automation.siemens.com.

Additional Keywords
Distributed configuration control, LLDP, activate IO device, topology detection, series machine, S7-1500, ET200 MP, ET200 SP, PROFINET, data records

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.