×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 91198957, Entry date: 05/19/2014
(0)
Rate

Regulation for protecting switching devices against overload and short-circuits

  • Entry
  • Associated product(s)

QUESTION:

How must switching devices be protected against overload and short-circuits?
What regulation determines whether miniature circuit breakers / circuit breakers or fuses have to be used?

 

 

ANSWER:

The regulation IEC 60364-4-43 is applicable here. It permits the use of both fuses and miniature circuit breakers or circuit breakers.
The permissible short-circuit protection of the control supply voltage of switching devices is frequently described in the operating instructions or in the device manual.
If not, no special rules have to be observed, and the planner of the installation has to dimension the protection according to the conditions of use (total current, cable length, cable cross-section, etc.).

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.